2020-08-31 8:35 AM
Hello,
I'm working on a project on STM32F769 DISCO Board in which I need to read and parse data from a .json file (3kb).
I tried using Nlohmann JSON.hpp library for data reading and parsing and, even if I do not have compilation problems (except for a certain number of infos), when I debug the program on the board, it seems that it is not able to read data from file. It is not clear if it is a memory problem or a problem with the library.
With the same library I managed to read and parse the same file correctly on a pc.
Any one has had a similar experience?
Can someone suggest a json library positively tested on a stm32 board (better if on a STM32F769 one).
Thanks
Have a nice day.
Pietro
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.