STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo-L433RC-P board with a BlueNRG-2 BLE

Hi I am testing the Nucleo-L433RC-P board with a BlueNRG-2 BLE interface. I configured the setup, but the BLE device is not being detected in the ST BLE app. Look at pic, Any modifications require are not ?   

Kumar123_0-1749551317611.png
Kumar123 by Associate III
  • 2315 Views
  • 12 replies
  • 1 kudos

Resolved! UART receive with HAL_UART_Receive_DMA

Hello everyone on the forum.I have created a UART DMA receive program with Nucle-H723.This time it is working properly, but sometimes it does not work properly.DMA set up in normal mode on UART4 RX.DMA initialization function of UART.void UART_DMA_In...

uart_dma01_02.png uart_dma02_02.png uart_dma03_02.png uart_dma04_02.png
Hey0256 by Associate II
  • 1698 Views
  • 2 replies
  • 0 kudos

Resolved! Unable to get ADC value on STM32N6570-DK

 Hi everyone,I’m currently working with the STM32N6570-DK board and trying to read an analog signal using the  ADC1/2 INP8 channel (PB10) using the MB1280C Fanout board (Pin 13) with STMOD+ connector. However, I'm consistently getting a value around ...

Resolved! STM32H7 + Zephyr + SIGTRAP 0xA05F0000

I'm running into an issue on two boards (an STM32H735 Discovery Kit) and a custom board with an H743. #include <stdio.h> #include <zephyr/kernel.h> int main(void) { while (1) { printf("Hello there, world!\n"); k_msleep(1000); } return 0; }If ...

i2pi by Associate II
  • 924 Views
  • 1 replies
  • 0 kudos

Resolved! Opamp on STM32U545 is impossible to read with ADC_IN8

Hello.I am finishing a project where I measure voltage with an ADC using the STM32L431 and, for greater accuracy, I am using the OPAMP (PA0 = ADC1_IN0_VINP and PA3 = ADC1_IN_VOUT). For the STM32L431 on the STM32CubeMX, when activating the OPAMP in "F...

EB by Associate II
  • 1305 Views
  • 3 replies
  • 1 kudos

Resolved! Hardfault after acessing FMC intyerface on STM32H753

MCU:        STM32H753XIH Tool:         STM32CubeIDE v1.18.1 FW Pkg:   FW_H7_V1.12.1   I have an in-house designed board that has an FPGA connected to the FMC bus. The FPGA uses a simple SRAM interface with Address (7:0), Data (31:0), Chip Select, Rea...

Hal56-GCI by Associate III
  • 2088 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.