STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Switch GPIO interruption

Hi, I have 3 interruption pins PA13, PA14 and PA15, I would like to enable one pin for interruption at a time and changing the interruption mode, I made this function, but I'm not sure if it's the right way to achieve that.void Switch(uint16_t PIN, u...

Vertinhol by Associate III
  • 908 Views
  • 2 replies
  • 0 kudos

STM32H743ZI2 ADC3 AND DMA

I am using NUCLEO-STM32H743ZI2. I try ADC3 + DMA, but I confuse ADC3 CLOCK, from cubeMx, I found THERE ARE 3 SOURCE (PLL2P,PLL3R,PER_CK) for adc clock, in manual, it mentioned SCLK and HCLK can be clock resource as well. In RCC adc clock selection, o...

yang hong by Associate III
  • 1773 Views
  • 2 replies
  • 0 kudos

Issue while adding padding to generated file

In my project I need to add padding to few flash address. I generated hex file which has flash data till 0x1000(Suppose) but I want to pad till 0x4000 with 0xFF. I am using below gcc commands but unable to get desired output.arm-none-eabi-objcopy --s...

Generate interrupt on center aligned mode at counter overflow

Hi,i am using STM32F334C6T.i try to set my PWM as Center Aligned mode and generate interrupt at counter overflow. my code as below.whatever i do in my code, i can not take just one interrupt which is counter overflow. everytime it generates two times...

AKOCA.1 by Associate II
  • 2985 Views
  • 4 replies
  • 0 kudos

Resolved! RTC backup registers after power off and on

Hi ST Community,I am using the RTC on the STM32l100RBT6 µC to display the date and time every hour. It is battery powered and therefore at some point i would have to change the batteries, therefore, the µC will lose power. I have thought of using the...

Resolved! Powering the 32L476GDISCOVERY board via USB USER

Hello all,I am trying to get started with a STM32DISCO board, like described here:https://www.st.com/en/evaluation-tools/32l476gdiscovery.html#documentationHowever, I can't get it powered.I use the USB USER connector to power it with my laptop.SB set...

NDecr.1 by Associate
  • 1298 Views
  • 1 replies
  • 0 kudos

No clock signal on PA5 bit(SPI1-SCK)

Hello,I'm learning to use the SPI module. I'm using an STM32F446RET development board. I want to configure the SPI1 module and send some message 'out into the world'(this means I only have one master devices which sends some bytes and no slave to rec...

PPopo by Senior
  • 7670 Views
  • 15 replies
  • 0 kudos

Resolved! HAL_I2C_Mem_Write_DMA sends only one byte

The blocking version (HAL_I2C_Mem_Write) works nicely, now I'm trying to use HAL_I2C_Mem_Write_DMA. Here are the settings as given in the configuration tool.The resulting code generated by the configurator (I removed some comments for brevity):static...

0693W000004IGU0QAO.png 0693W000004IGR1QAO.png 0693W000004IGYfQAO.png 0693W000004IGhcQAG.png
iforce2d by Associate III
  • 3576 Views
  • 5 replies
  • 0 kudos

Resolved! Possible to disable SPI clock output?

I'm using SPI to output a signal for addressable RGB LEDs, as described here. https://innomatic.home.blog/2018/12/24/ws2812sk6812-control-with-spi-and-dma/Since this signal requires only the MOSI pin, it would be great to be able to use the CLK pin f...

iforce2d by Associate III
  • 2722 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.