2020-10-02 1:13 AM
In my project I need to add padding to few flash address. I generated hex file which has flash data till 0x1000(Suppose) but I want to pad till 0x4000 with 0xFF. I am using below gcc commands but unable to get desired output.
arm-none-eabi-objcopy --set-start 0x08000000 --pad-to=0x4000 --gap-fill=0xFF BootloaderDiscovery.elf BootloaderDiscovery.bin -O binary
any suggestions ?
2020-10-02 7:50 AM
> --set-start 0x080000000
0x080000000 = 0x8000 0000 = not the start of the flash. You want 0x0800 0000.
2020-10-02 8:01 AM
Oh that's typo. I updated, Still same result.
arm-none-eabi-objcopy --set-start 0x08000000 --pad-to=0x4000 BootloaderDiscovery.elf BootloaderDiscovery.bin -O binary
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.