STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

timer

I am using NUCLEO-H743ZI2. I am trying timer to generate pulse using TIM_OCMODE_TOGGLE channel 1. my timer clock is 100MHz, I set pre-scaler as 9 and channel 1 pulse as 9 as well. It seems it is difficult to get pulse, except I add more count on chan...

yang hong by Associate III
  • 892 Views
  • 3 replies
  • 0 kudos

Cable length limitation for SPI run at 40MHz ???

I had trouble to activate SPI communication with SPI in 40MHz frequency in 55cm long cable , even I modified output speed to "Very high speed" . Is any other register that I need to set to support high speed clock in long length cable ? 55cm long cab...

AShiu.1 by Associate
  • 1505 Views
  • 1 replies
  • 0 kudos

Several question regarding STM32Fx (TIMx,DMA,ADC)

Hello,I have few questions regarding the TIMER capabilities confgured as input capture. According to the reference manual, the direct input capture of TIMxCH1 in conjunction with a TMxCH2 which is configured as "indirect input capture mode" along ...

PButc.1 by Associate II
  • 2404 Views
  • 3 replies
  • 0 kudos

Use STM32H743II with an external ldo for vcore @ 400MHz

We would use a STM32H743II with an external ldo for vcore. In the datasheet are tables (page 114, table 31) with regulator on but no tables with regulator off.In the datasheet at page 114 is a table (table 31) for maximum current vs. junction tempera...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.