STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI max frequency test

Hey,I would like to use an ADC LTC2315,in maximum SPI interface (87.5Mhz Fclk).Does anyone tried to work with the STM32H743 In SPI At this Frequency, or more?From DS, in master mode Channel 1 can work in Max of 133MHz, hope it really does.Moreover, c...

Pkats.1 by Associate II
  • 1164 Views
  • 1 replies
  • 0 kudos

Resolved! Latching comparator output

I'm building an overcurrent protection device based on an STM32F301C8, using COMP2 to compare an analog signal from a hall sensor against the DAC1 output value.Now I'd like to generate a latching error signal that will remain asserted when the overcu...

Littlefs and flash lifespan calculation ?

Hi,In my office, I use a custom STM32F767GTx card with a QSPI N25Q128A flash memory.I use littlefs to create, write and read files.My software works well, I monitor some inputs and store these values in a file.Every 24 hours, I have a 200 kbytes file...

LRABO.1 by Associate II
  • 2958 Views
  • 1 replies
  • 0 kudos

Where is the NUCLEO-L552ZE-Q default binary?

I'm talking about the firmware with which the Nucleo comes ex factory. It's not among the compiled binaries (https://www.st.com/en/evaluation-tools/stm32-discovery-kits.html#resource click on Binary resources - no direct link courtesy of the idiotic ...

Resolved! For STM32H745XI-Disco board are there example source code for initializing and using CRC , SDRAM and also using the EMMC 4GB flash .

Hi ,We need to develop driver for 4GB EMMC flash and SDRAM .For STM32H745XI-Disco board is there example source code for initializing and using CRC , SDRAM and also using the EMMC 4GB flash .Thanks In Advance

STM32L412: When I turn the reset (physical) switch, the µC jumps into the DFU bootloader, although it isn't supposed to

Hi there!I have a weird problem, where I'm a bit lost, probably also due to my limited knowledge of assembly. So I am trying to write a function (which is called using a very secret pattern) which sets a magic number and soft resets the microcontroll...

SPI Communication with STM32G031 using HAL

Hello,I tried to configure the STM32G031K8 Nucleo Board using CubeMX to send a request to an attached sensor using SPI1. To my request (2 bytes) the sensor should answer with 4 bytes. I configured the data size to 8 bits and the clock parameters core...

CLau.1 by Associate
  • 1272 Views
  • 0 replies
  • 0 kudos

Resolved! How to use HAL i2c and math.h in same project?

Hi everyone! I am using STM32F4 and IMU to read gyro and accelerometer, and than calculate IMU's euler angles. I can get data from IMU it is OK but when I try to add something from math.h program stops working but it also don't gives error or warninn...

0693W000004JjWRQA0.png 0693W000004JjZ5QAK.png
MDoğr.1 by Associate II
  • 1625 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.