2020-10-14 7:43 PM
I had trouble to activate SPI communication with SPI in 40MHz frequency in 55cm long cable , even I modified output speed to "Very high speed" . Is any other register that I need to set to support high speed clock in long length cable ? 55cm long cable is not possible to support 40MHz ,?
2020-10-14 8:14 PM
A 55cm cable is pretty long for 40MHz single ended SPI. I would not expect it to work okay without attention to impedance matching and proper terminations. It's not a matter of chip support, it's a matter of signal integrity in the cable, after the signal leaves the chip.
A differential signal in a shield cable would do better (e.g. USB).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.