STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Handle gesture event not working on STM32F0 platform ?

On My STM32FO platform, i'm implemented touchgfx swipe container with 4 pages.I want to change page with a swipe on the display.But this not working. A touch ( swipe ) on the display called the handleClickEvent function of the swipe container.but nev...

PIRRI.1 by Associate II
  • 845 Views
  • 0 replies
  • 0 kudos

Stm32f407 discovery board issues

I am new to coding. I brought new stm32f407 discovery board. Intially their is no issue with debugging for target. But now ld1 ld2 are continuously glowing and ld3 ld4 ld5 ld6 are not glowing when i connect the board for pc and when a usb is connect ...

Detect I2C device has stopped working

Using STM32L4 with DS3231. Using LL interrupts to communicate with device.Is there any way using interrupts to detect the device has stopped working. stopped working in the sense that that device is not ACK ng or has lost Vcc. not as in device functi...

Hp.14 by Associate II
  • 3542 Views
  • 4 replies
  • 0 kudos

Resolved! My SPI analyzer is different from what I send.

Dear ST Hello,I am coming back to you because the my spi frame I am sending is not the same I am watching on the oscilloscope,My spi configuration is: /* USER CODE BEGIN SPI3_Init 0 */   /* USER CODE END SPI3_Init 0 */   /* USER CODE BEGIN SPI3_...

0693W000004KDFjQAO.png

Sampling 16 ADC channels (multichannels) on STM32G070 RB

Hello COmmunity i want to sample 16 ADC channels on my STM32 G070 board i tried with DMA conversion and using simple poll for conversion but i am not getting accurate o/p (required o/p). Please do let me know if i missing anything/* USER CODE BEGIN H...

AKhai.1 by Associate
  • 1193 Views
  • 1 replies
  • 0 kudos

Resolved! What do Events from EXTI controller use for?

In the STM32F070, EXTI0_15 come from GPIOs, EXTI17 comes from RTC Alarm Event, EXTI18 comes from USB wakeup Event, EXTI19 comes from RTC Tamper and TimeStamp Event, EXTI20comes from RTC Wakeup Event. Where are destination of EXTIs? or Where are EXTIs...

FAlle.1 by Associate II
  • 2011 Views
  • 3 replies
  • 0 kudos

Wrong MCU frequency only while debugging

Problem definition:PLLCLK frequency is different (wrong) in debugging mode only.Two empty projects were created using CubeMX 6.0.1 and 4.25.1 as a reference.running exactly the same main.c where only HSE and MCO are enabled outputs different results....

MUrbs.1 by Associate
  • 1042 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.