2020-10-19 6:32 AM
Problem definition:
PLLCLK frequency is different (wrong) in debugging mode only.
Two empty projects were created using CubeMX 6.0.1 and 4.25.1 as a reference.
running exactly the same main.c where only HSE and MCO are enabled outputs different results.
CubeMX 4.25.1 code runs as expected and MCO outputs 216MHz in both regular operation and while debugging
CubeMX 6.0.1 runs incorrectly. Under regular operation the frequency is 216MHz as expected, however in debugging mode the MCO output is 189MHz. It was double checked with timers and comms. Everything is running slower while in debugging mode.
Same thing happens with 12MHz and 25Mhz HSE oscillators.
Test code:
static void ConfigureHSE(void)
{
RCC->APB1ENR |= RCC_APB1ENR_PWREN; // Power interface clock enable
while ((RCC->APB1ENR & RCC_APB1ENR_PWREN) != RCC_APB1ENR_PWREN)
{
};
PWR->CR1 |= PWR_CR1_VOS; // Voltage scaling = range 1
while ((PWR->CR1 & PWR_CR1_VOS) != PWR_CR1_VOS)
{
}; // Waits until scaling is ready
FLASH->ACR = ( FLASH_ACR_PRFTEN | // Prefetch enable
FLASH_ACR_LATENCY_7WS); // FLASH 4 wait states
RCC->CR &= 0;
RCC->CR |= RCC_CR_HSEON; // Enables HSI clock
while ((RCC->CR & RCC_CR_HSERDY) != RCC_CR_HSERDY)
{
}; // Waits until HSI is stable
RCC->PLLCFGR = ( RCC_PLLCFGR_PLLSRC_HSE | // PLL SRC = HSI
(12u << RCC_PLLCFGR_PLLM_Pos) | // PLL_M = 12
(432u << RCC_PLLCFGR_PLLN_Pos) | // PLL_N = 432
(0u << RCC_PLLCFGR_PLLP_Pos) | // PLL_P = 2
(2u << RCC_PLLCFGR_PLLQ_Pos)); // PLL_Q = 2
RCC->CFGR = 0;
RCC->CFGR |= RCC_CFGR_HPRE_DIV1;
RCC->CFGR |= RCC_CFGR_PPRE1_DIV4;
RCC->CFGR |= RCC_CFGR_PPRE2_DIV2;
RCC->CR |= RCC_CR_PLLON; // Enables the PLL
while (!(RCC->CR & RCC_CR_PLLRDY))
{
}; // Waits until PLL is stable
RCC->CFGR &= ~RCC_CFGR_SW;
RCC->CFGR |= RCC_CFGR_SW_PLL;
while (!(RCC->CFGR & RCC_CFGR_SWS_PLL))
{
};
InitializeMCO();
}
/* Displays MCO on PA8 */
static void InitializeMCO(void)
{
/* Main clock output (MCO): */
RCC->CFGR &= ~RCC_CFGR_MCO1_Msk;
RCC->CFGR |= (0x3 << RCC_CFGR_MCO1_Pos);
RCC->AHB1ENR &= ~RCC_AHB1ENR_GPIOAEN;
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOAEN;
GPIOA->MODER &= ~GPIO_MODER_MODER8;
GPIOA->MODER |= GPIO_MODER_MODER8_1;
GPIOA->OTYPER &= ~GPIO_OTYPER_OT_8;
GPIOA->PUPDR &= ~GPIO_PUPDR_PUPDR8;
GPIOA->OSPEEDR &= ~GPIO_OSPEEDER_OSPEEDR8;
GPIOA->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR8_1;
GPIOA->AFR[0] &= ~GPIO_AFRL_AFRL0;
}Thank you in advance for any tips how to fix this
2020-10-19 6:39 AM
Not sure, the MCO isn't rated at ~200 MHz output, usually needs dividing down.
Would recommend you dump out the RCC registers and compare-n-contrast.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.