STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H750vb want create stldr ,I need help

I learn the lesson,but it STM32F769I-Discovery board​this video use file but i can't find it.i look this video already copy the file,add the project,is true?i guess new project,copy the file ,add project,addtion, Where there is need to modify?thanks,...

Qqixi.1 by Associate II
  • 1164 Views
  • 1 replies
  • 1 kudos

Resolved! Can not write data in flash of STM32G030C8T6

This is my code;it when run to the code in the picture, the MCU will deadvoid Flash_Test(void){  U32  Write_Addr = FLASH_USER_START_ADDR; //FLASH_USER_START_ADDR=((uint32_t)0x0800E000)  uint64_t data64=0x1234567812345678;  EraseInitStruct.TypeErase ...

Pzhu.1 by Associate II
  • 1693 Views
  • 2 replies
  • 0 kudos

STM32F407 blink project not working

I'm trying to figure out if the board is functional by trying the simple on board LED blink project, the board is STM32F407VGT6 and IDE is Keil uVision5. I'm using the code below:#include "stm32f4xx_hal.h"   void configureLEDpins(void); void msDelay(...

ATAB.1 by Associate
  • 1023 Views
  • 0 replies
  • 0 kudos

Resolved! UART CONFIGURATION PIN DETAILS

Hi Team I want to interface UART on my STM32H7B3I-DK device I am aware of the code that needs to be generatedusing the ide for UART ,I am not sure on the pin connections that needs to be made inorder to receive the data Can you please let me know the...

DRAME.1 by Associate II
  • 1208 Views
  • 2 replies
  • 0 kudos

STM32F405 unable to flash, damaged flash?

Hello,Yesterday I was working on a device that uses the STM32F405RG chip, functionally it's a Vedder ESC, when the computer no longer recognized that I had the USB plugged in to the board. After a bit of troubleshooting I thought I should reflash th...

NRich.1 by Associate II
  • 2987 Views
  • 3 replies
  • 0 kudos

Resolved! STM32L010K4T loses flashed program after reset or power off

Hi,I'm quite new to STM32 MCUs as I just switched from PSoC MCUs. I'm using a STM32L010K4T6 and I cannot get it to work as the problem seems to "disappear" after reset or power off. I went through the configuration (I'm using STM32CubeIDE) and I cann...

DKjel.1 by Associate
  • 1892 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 digital signal processing?

Hello everyone,I am using an STM32L4 MCU and I am trying to create a digital bandpass filter for the data being received on the ADC channel. Is there any standard library which would enable me to do this? If there is not, are there any resources (app...

MCrew.1 by Associate III
  • 2365 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.