2020-10-12 12:30 PM
Hi Team
I want to interface UART on my STM32H7B3I-DK device I am aware of the code that needs to be generated
using the ide for UART ,
I am not sure on the pin connections that needs to be made inorder to receive the data
Can you please let me know the pin connection details to receive data via uart(TX RX GND) on STM32H7B3I-DK
Thank you
Deepak R
Solved! Go to Solution.
2020-10-12 12:42 PM
Which UART? The VCP or Arduino?
VCP USART1 (TX PA9 / RX PA10)
D0 USART3_RX PB11
D1 USART4_TX PH13
Note the Arduino uses TWO different USARTs
2020-10-12 12:42 PM
Which UART? The VCP or Arduino?
VCP USART1 (TX PA9 / RX PA10)
D0 USART3_RX PB11
D1 USART4_TX PH13
Note the Arduino uses TWO different USARTs
2020-10-21 2:48 PM
I am not sure I want to receive the data bu UART on my board and use those values in my program
can you please help me on how to connect I am not sure about connecting aurdino on to this board Is there any document that explains the interfacing can you please guide what arduino version i should buy
I know arduino has the inbuilt program to collect data after doing this how can i get read the data STM32 program
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.