2020-10-21 7:19 PM
Our project want to use the 4GB eMMC NAND Flash on STM32F103RC or STM32F412VE.
The eMMC architecture of NAND flash support revision , below. It just require to over the MMC standard 4.41 / 5.1.
Could the STM32F103RC or STM32F412VE support 4GB eMMC NAND flash?
2020-10-21 7:24 PM
Both of them have the hardware to support 4GB eMMC. The HAL support may not be complete. Last I checked the F4 only supported up to 2GB.
2020-10-21 9:20 PM
Yes, both F1 and F4 should be capable of accessing an eMMC device. You'll be responsible for implementing the driver.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.