STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can ADC1 analog watchdog trigger TIM8?

Is it possible for any of the analog watchdogs of ADC1 to be used to trigger TIM8? I would like to stop a PWM generated using TIM8 when an ADC1 conversion crosses a threshold. Table 251, Interconnect to the tim_etr input multiplexer seems to indicate...

galens by Associate II
  • 1800 Views
  • 3 replies
  • 0 kudos

STM32F412 clock config issue

I made a custom board with an STM32F412RE chip and I can program it, and step through my code, but when I try to initialize my system clock I get stuck in a while loop that times out that I don't think should.[Here](https://imgur.com/a/Jqa1JmG) is my...

ABuja.1 by Associate II
  • 1782 Views
  • 2 replies
  • 0 kudos

STM32 as I2C slave - sporadic errors - how to diagnose?

EDIT: Note change of direction of things in 3rd post.I have a stm32f091, which has a program that basically runs one mainloop that triggers ADC measurements and polling values from i2c chips using the i2c2 peripheral in master mode. ADC uses a DMA ir...

SKled.1 by Senior II
  • 2015 Views
  • 2 replies
  • 0 kudos

STM32F072RB Jitter/Delay

Small delays occur in projects and tests. The delays are usually about 6us. They also occur with simple calculations. What can be the reason? I have already tested with a new project without functionalities.

MF.2 by Associate
  • 3434 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.