STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to generate udp_echoclient.c in STM32 H743

HiI'm trying to implement STM32 F429 code into STM32 H743.The previous code works fine, so I'm trying the code in STM32 H743 as well.I mimic most of settings, but failed to generate udp_echoclient.c file.Can somebody help me out with this?Thank you i...

SHong.5 by Associate II
  • 738 Views
  • 0 replies
  • 0 kudos

Resolved! HAL_TIM_PeriodElapsedCallback() refuses to trigger

GreetingsI have attempted to write an application, to toggle the LD4 LED (On PD12) on the STM32F407VGTx Discovery board. I am toggling the LED, on interrupt, when the timer overflows. I have placed the HAL_GPIO_Toggle() in the HAL_TIM_PeriodElapsedCa...

LSlat.1 by Associate II
  • 8423 Views
  • 6 replies
  • 2 kudos

interrupt on receiving bytes via SPI HAL

help me please. working in stm32cubeide. I can not enable interrupt on receiving bytes via SPI via HALmain.c/* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h"   /* Private var...

k.s.corp by Associate II
  • 3649 Views
  • 7 replies
  • 0 kudos

Resolved! STM32L0 current consumption jumps from 650uA to 2-8mA

Hi,I'm working on a low power project that my micro-controller can only have 1mA in 2.7V.My micro-controller is stm32l051c8 and its works nice with its peripherals (ADC and Timer) and its current consumption is about 0.65 mA. But After working for A ...

sshaf.1 by Associate
  • 2176 Views
  • 4 replies
  • 1 kudos

STM32 I2C not receiving further bytes

Hello I am beginner to MCU, I have set STM32F407 Discovery as a master on I2C communication with nucleo STM32F446RE as a slave. PC host connected to the STM32F407 via UART. The code for the master ischar RecBuff [20]; while (1) { HAL_UART_Receiv...

0693W000005BNhPQAW.jpg
HGhaf.1 by Associate
  • 978 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.