cancel
Showing results for 
Search instead for 
Did you mean: 

How to solve Imprecise data access violation (IMPRECISERR). STM32H743 / LWIP / memp_init();

SHong.5
Associate II

Hi

I'm new into MCU and currently using STM32 H743.

My code is facing HardFault_Handler every time I run.

After I debugged several times, I found the root error from LWIP.

The Fault Analyzer saids, it's Imprecise data access violation(IMPRECISERR) from BUS fault.

However, I have no idea how to deal with this.

Here's the code below

Middlewares > Third Party > LwIP > src > core > init.c

void

lwip_init(void)

{

........

mem_init();

memp_init(); <------------------- THIS ONE (goes into HardFault_Handler loop)

pbuf_init();

netif_init();

.......}

And Register Content During Fault Exception saids.

NAME VALUE

sp (MSP) 0x2001ff68

r0 0x30054000

r1 0x1010108

r2 0x20001a78

r3 0x30044000

r12 0x0

lr 0x800cd8b

pc 0x800a806

xpsr 0x1000000

Can anybody help me out with this?

Thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

Are your clock settings valid? What statement in memp_init triggers the hard fault?

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Super User

Are your clock settings valid? What statement in memp_init triggers the hard fault?

If you feel a post has answered your question, please click "Accept as Solution".

oh... thanks a lot. As I changed clock settings, the error is immediately gone.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.