2021-01-07 9:01 PM
Hello,
I configure my DMA in Normal mode. Here is my code:
void DMA1_Channel3_IRQHandler(void){ // USART3_RX
unsigned char CheckSum[2];
Var1=Var1+1;
if(Var1>1000){Var1=0;}
if(Buffer[0]==89 && Buffer[26]=='\n')
{
Var2=Var2+1;
if(Var2>1000){Var2=0;}
}
DMA_ClearITPendingBit(DMA1_IT_TC3);
DMA_ClearITPendingBit(DMA1_IT_TE3);
DMA_Cmd(DMA1_Channel3, DISABLE);
DMA_SetCurrDataCounter(DMA1_Channel3,sizeof(Buffer));
}
void EXTI9_5_IRQHandler(void){
if (EXTI_GetITStatus(EXTI_Line5) != RESET)
{
if(GPIO_ReadInputDataBit(GPIOA,GetPosition)==0 )
{
DMA_SetCurrDataCounter(DMA1_Channel3,sizeof(Buffer));
DMA_ClearITPendingBit(DMA1_IT_TC3);
DMA_ITConfig(DMA1_Channel3,DMA_IT_TE, ENABLE);
USART_ITConfig(USART3, USART_IT_ERR, ENABLE);
USART_DMACmd(USART3, USART_DMAReq_Rx, ENABLE);
DMA_Cmd(DMA1_Channel3, ENABLE);
GPIO_ResetBits(GPIOA,SendSignalPosition);
}
else
{
GPIO_SetBits(GPIOA,SendSignalPosition);
DMA_Cmd(DMA1_Channel3, DISABLE);
}
EXTI_ClearITPendingBit(EXTI_Line5);
}
}Before each transmission, The transmitter change the PA.5 to low level , and if the receiver changes its SendSignalPosition pin(start DMA), the transmitter start transmitting and wait for 50us after all bytes being transferred.
This code works fine until I send some packages to the transmitter with DMA(TX) from the receiver. After sending some packages, the DMA looses the input sequence. I checked the variable Var1 and Var2 and I found out that Var1 is increasing ( the DMA is collecting the input bytes) but Var2 doesn't change after losing the input string sequence.
I need to know why this is happening while before each transsmison I disable/enable the DMA.
In addition, I've checked the Buffer[0] and I've seen that it contains the last character of the previous string. It seems the last character maintain in the buffer while the DMA is disabled.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.