STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

When will STM32G0x0 be available?

Everywhere I check online, I cannot find any STM32G070 chips. I'm looking to up my game from 8-bit AVR to 32 ARM MCUs that stay in the same price range.

EFrei.2 by Associate
  • 1071 Views
  • 1 replies
  • 0 kudos

Which parts of an .ELF file go into the .bin file?

(since I am getting "Error while parsing Rich Text Content" in the saved post all the time, even though in the EDITOR everything renders just fine, I dumped the text in there without nice formatting)---------------------------------------------------...

SKled.1 by Senior II
  • 5648 Views
  • 5 replies
  • 0 kudos

Mount problems with SD Card greater than 1G

Dear all,i'm developing an application with STM32F750N8 and I'm using SDMMC peripheral (48MHz clock, rising clock transition, no prescaler and hardware flow control) and FatFs library, for read and write the micro SD Card.I tried to use a 1GB SD Card...

Luca G. by Associate III
  • 4073 Views
  • 5 replies
  • 0 kudos

Resolved! STM32F303 ADC1 calibration stuck

HiI'm porting my STM32F103 code to the STM32F303, and noticed the significant difference in the ref manual regarding the ADC module. Being a beginner in STM32 MCUs, I'm struggling to get my calibration run correctly.I feel like I am doing as I'm supp...

AAnth.1 by Senior
  • 2831 Views
  • 3 replies
  • 0 kudos

STM32F103 UART2 not Receiving data

Hi all,I am facing one issue with STM32F103 UART2 receiving side, it is transmitting data but not receiving. i just configured MCU with CUBEMX and changed only main.c file.Configuration and main.c are attached here.I just made a very simple program "...

sanju by Senior
  • 2086 Views
  • 2 replies
  • 0 kudos

STM32L051C8 uses ADC to measure voltage value error is 50mV

STM32L051C8 uses ADC to measure the voltage value. The measured voltage value of the AD pin is 0.432V,VCC=3.335V, and the voltage value obtained through AD collection is 0.48V; there is an error of 50mV, and the ADC part of the program and hardware a...

0693W000006I984QAC.png 0693W000006I99RQAS.png
*于.1 by Associate II
  • 1884 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.