STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can't access STM32L552 after setting SRAM2-RST to 0

I've been trying to run the SBSFU example from STM32Cube_FW_L5_V1.2.0.The option bytes I set initially were:TZEN=1DBANK=1 (was already 1)SECWM1_PSTRT=0x0 and SECWM1_PEND=0x7fSECWM2_PSTRT=0x1 and SECWM2_PEND=0x0.That allowed me to load SBSFU bootloade...

tosa by Associate
  • 1727 Views
  • 2 replies
  • 0 kudos

Typo in several documents (wait sates)

I came across "wait sates" (with missing "t") in RM0316 rev.8, but just for the laugh I threw it into google (https://www.google.com/search?q="wait+sates"+site%3Ast.com ), and... lo and behold, this appears to be a quite often repeated typo, at least...

Resolved! Max current possibly sourced from a DAC pin?

Hello. I would like to know how much current a DAC pin is able to source. The STM32G081 datasheet indicates "Output current sourced by any I/O and control pin = 15mA". Is this 15mA also an upper limit to a DAC sourcing pin? The STM32G081 datasheet al...

JLemi by Associate III
  • 3717 Views
  • 3 replies
  • 0 kudos

Resolved! TIM2 freeze on ARR register value changed STM32H743ZI2

Hi. I'm working on project where I need short pulses with precise periods generated in audio ranges (10 - 20kHz). So I decided to choose TIM2 and using it in PWM mode. I'm using HAL library and configuration code generated by CubeMX:void MX_TIM2_Init...

Stm32f407 discovery board real or fake?

I have bought new STM32F407 DISCOVERY BOARD and I got blue board STM32F407 Discovery board so is it real or fake, while connecting via mini B cable also memory showing only approx. 20-30kb of space in it so please confirm it as real or fake?

SVerm.3 by Associate III
  • 2396 Views
  • 6 replies
  • 0 kudos

Resolved! All 0x00 in STM32G4 flash? Is it can be recover?

I am testing STLINK Utility's Automatic Mode for mass-production,I set read out protection in option byte from level0 to level1(I have never set it to level2,for its irreversibility),so I just plug in and out the STLINK acting as the operation of mas...

0693W000006ICNgQAO.png 0693W000006ICNlQAO.png 0693W000006ICM0QAO.png 0693W000006ICOyQAO.png
ZYu.1 by Associate III
  • 3030 Views
  • 3 replies
  • 0 kudos

Resolved! How to read Timer Capture triggered by software

I have an application where I am using an external signal to trigger TIM8_CH1 to do a capture and generate a DMA interrupt where I then store the counter value. I want to perform a similar action on an internal firmware (FW) signal. I want to store t...

BTrem.1 by Senior II
  • 1950 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.