STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am using the STM CubeIDE with a Nucleo L476RG dev board. When I first generated a project I was able to download it to the card and debug. then for some reason I started getting an error saying the arm-none-eabi-gdb.exe has stopped working.

I am able to open an example project and debug that without issues. I have tried regenerating my project, generating a new project, and even reinstalling the tool and generating a new project, but I still get the same error on debugging. I can still ...

BCrow.1 by Associate II
  • 1920 Views
  • 3 replies
  • 0 kudos

stm32l0 with lptim generate PWM + RTC every 10 sec and stop mode

hello,I am using stm32l0 in low power modeconfigure RTC to wakeup from stop mode each 10 sec , I use LPTIM to generate PWMmy problem is that I noticed the led is starting to blink for every 10 sec +- after a while what seems to be the problem? ( I ...

M4D by Associate II
  • 876 Views
  • 0 replies
  • 0 kudos

Why the STM32F0 and STM32F1 Many MCUs out of stock?

Hello there. For some time now, STM32F0 and STM32F1 series many MCUs have been experiencing stock problems.  STM32F030, STM32F042, STM32F072 and STM32F103 series many mcu have stock problems. It seems that there is no stock at suppliers like Digikey,...

FYOL.1 by Associate II
  • 2051 Views
  • 3 replies
  • 0 kudos

MATLAB Simulink support packages for ST MCU's

In MATLAB Simulink 2020b Software, I saw that support packages are available for STM32 F4, STM32F746G, STM32F769I; But in this document, "https://my.st.com/resource/en/data_brief/stm32-mat-slsh-target.pdf", it is mentioned, the following controller...

VVija.1 by Associate II
  • 1032 Views
  • 0 replies
  • 0 kudos

Resolved! What pins are available for GPIO on STM32F429I-DISCO?

My initial thought was that while some pins are connected to other peripherals on the discovery board, that they may still be used for GPIO. Is this true, or can a pin not be used for GPIO if connected to a peripheral, even if that peripheral is not ...

MChap.1 by Associate
  • 1390 Views
  • 2 replies
  • 0 kudos

Resolved! NSS the output ignores the settings, and according to the waveform, the outputs are in the hiz state, because you can see the leads that are not damped by pressing to the ground. (STM32F303)

NSS the output ignores the settings, and according to the waveform, the outputs are in the hiz state, because you can see the leads that are not damped by pressing to the ground. (STM32F303)   //   Bit 4 FRF: Frame format   //   0: SPI Motorola mode ...

Resolved! STM32H7 (dual core) ADC1/2/3 ressource split

Hello,I have one question regarding the ADC1/2/3 cores for the STM32H7 (dual core solution). Let's say, I would like to split few ADC channels between both ADC cores and Cortex cores. Is it possible to assin channels 1,2,3 for ADC1 core (regular grou...

PButc.1 by Associate II
  • 1218 Views
  • 1 replies
  • 0 kudos

Unnecessary hardfault due to button press on system wakeup pin.

We are trying to build a USB Data Logger We are facing some issue while being in run mode. Initially system is in standby mode and can be woken using button press (connected to system wakeup 1). On 5 sec press system/mcu starts logging data into flas...

JKSah by Associate II
  • 3032 Views
  • 6 replies
  • 0 kudos

PWM Timer and GPIO level

Hello,I'm using a STM32F091 with TIM2 configured in PWM mode.(and CH1-CH2 connected to an output)After some hundreads of milliseconds, I have to stop the PWM by setting CCRx at 0. And reenable later.So far so good.But to improve my working, I would t...

PCu1 by Senior
  • 2629 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.