STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NRF24L01 module with STM32

Hi,Is there anyone is using NRF24L01 module with STM32??Please do share the working library files for transmitter & receiver..Thanks in advance..

Bs.1 by Associate II
  • 2845 Views
  • 3 replies
  • 0 kudos

SDIO CMD53 gets into unexpected state

Hi Support Forum,I am using STM32H743ZI part with SDIO configured as Master and connected to SDIO slave which is a Wi-Fi module.In this case high speed bidirectional data transfer happening  Tx -20Mbps while Rx with 1024bytes/sec.As soon as data tran...

CMoul.1 by Associate
  • 1432 Views
  • 0 replies
  • 0 kudos

Resolved! STM32L1xx RTC counter

RTC used the LSE with 32768Hz oscillator and is configured for this option.While DBP bit is set RTC counter is stopped . Is it true or false?

costi by Associate III
  • 2449 Views
  • 4 replies
  • 0 kudos

STM32L4P5 SAI2-A no signal output issue

Dear all,I hope I can receive som help from you. I'm struggling since a couple of days with SAI2 block A on the mentionned MCU.I am using STM32CubeIDE and I have configured it using HAL library in master mode with MCLK output.When I try to send some ...

SaB0tAgE by Associate II
  • 1831 Views
  • 5 replies
  • 0 kudos

digital potentiometer set via i2c with stm32f303ze

I am currently working on controlling a digital potentiometer using i2c with the STM32f303Ze. According to the datasheet of the DigiPot you can send different bits to make adjustments. after a lot of trial and error the voltage still didn't change.co...

MSchm.6 by Associate
  • 2193 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F746G-DOSCO, FLASH

HelloI want to write to FLASH variable uint32_t time at power off. Which signal to use for this? greetingsAndrzej

AD�?b by Senior
  • 2352 Views
  • 5 replies
  • 0 kudos

Resolved! DMA to external SRAM misses bytes part-way through transfer

I have a stm32f427 with 1Mx16 external SRAM and SDMMC.I am reading the SDMMC by DMA into the SRAM in two blocks of 512 bytes into a 1024 byte buffer.The SRAM is mapped from 0x64000000 - 0x641fffff. Address and data are not multiplexedI have now disco...

Danish1 by Lead III
  • 2549 Views
  • 2 replies
  • 0 kudos

Resolved! Sending one byte via SPI STM32G474

I need to send data one byte at a time via SPI. After transferring the byte, I set "Chip Select" from the program to state 1. I track the end of the transfer by the BSY bit in the SPI_SR register. But the microcontroller transmits two bytes, the firs...

Akoli.1 by Associate II
  • 4057 Views
  • 6 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.