2020-12-20 11:27 PM
Hi,
Is there anyone is using NRF24L01 module with STM32??Please do share the working library files for transmitter & receiver..
Thanks in advance..
2020-12-21 5:13 PM
Try a google search for example stm32 nrf24l01 github
2020-12-21 8:35 PM
Ok. Will check.
2021-01-29 11:10 PM
hi...
I found nrf24l01 library on github..
I included it in my, but still I am facing problem during reception.
At transmitter side I found TX_DS bit set. But at receiver side it doesn't give the true result for NRF24_available().
main()
{
MX_GPIO_Init();
MX_SPI1_Init();
MX_USART2_UART_Init();
NRF24_begin(GPIOB, CSN_Pin, CE_Pin, hspi1);
nrf24_DebugUART_Init(huart2);
NRF24_stopListening();
NRF24_openWritingPipe(TxpipeAddrs);
NRF24_setAutoAck(false);
NRF24_setChannel(NRF_CH_Select());
NRF24_setPayloadSize(32);
while(1)
{
MyTxBuf[0] = 1+ 0x30;
MyTxBuf[1] = 1;
if(NRF24_write(MyTxBuf,32)) //data send over RF
{
HAL_UART_Transmit(&huart2, (uint8_t *)"Transmitted successfully\r\n", strlen("Transmitted successfully\r\n"), 50);
HAL_UART_Transmit(&huart2, &MyTxBuf[0], sizeof(MyTxBuf[0]),10);
HAL_UART_Transmit(&huart2, &MyTxBuf[1], sizeof(MyTxBuf[1]),10);
}
}
}
I have attached the library file.
Please have a look..
If any thing wrong in that...
/*
Library: NRF24L01 software library for STM32 MCUs
Written by: Mohamed Yaqoob
Date written: 25/10/2018
Last modified: -/-
Description:
*/
#define _BV(x) (1<<(x))
/* Memory Map */
#define REG_CONFIG 0x00
#define REG_EN_AA 0x01
#define REG_EN_RXADDR 0x02
#define REG_SETUP_AW 0x03
#define REG_SETUP_RETR 0x04
#define REG_RF_CH 0x05
#define REG_RF_SETUP 0x06
#define REG_STATUS 0x07
#define REG_OBSERVE_TX 0x08
#define REG_CD 0x09
#define REG_RX_ADDR_P0 0x0A
#define REG_RX_ADDR_P1 0x0B
#define REG_RX_ADDR_P2 0x0C
#define REG_RX_ADDR_P3 0x0D
#define REG_RX_ADDR_P4 0x0E
#define REG_RX_ADDR_P5 0x0F
#define REG_TX_ADDR 0x10
#define REG_RX_PW_P0 0x11
#define REG_RX_PW_P1 0x12
#define REG_RX_PW_P2 0x13
#define REG_RX_PW_P3 0x14
#define REG_RX_PW_P4 0x15
#define REG_RX_PW_P5 0x16
#define REG_FIFO_STATUS 0x17
#define REG_DYNPD 0x1C
#define REG_FEATURE 0x1D
/* Bit Mnemonics */
#define MASK_RX_DR 6
#define MASK_TX_DS 5
#define MASK_MAX_RT 4
#define BIT_EN_CRC 3
#define BIT_CRCO 2
#define BIT_PWR_UP 1
#define BIT_PRIM_RX 0
#define BIT_ENAA_P5 5
#define BIT_ENAA_P4 4
#define BIT_ENAA_P3 3
#define BIT_ENAA_P2 2
#define BIT_ENAA_P1 1
#define BIT_ENAA_P0 0
#define BIT_ERX_P5 5
#define BIT_ERX_P4 4
#define BIT_ERX_P3 3
#define BIT_ERX_P2 2
#define BIT_ERX_P1 1
#define BIT_ERX_P0 0
#define BIT_AW 0
#define BIT_ARD 4
#define BIT_ARC 0
#define BIT_PLL_LOCK 4
#define BIT_RF_DR 3
#define BIT_RF_PWR 6
#define BIT_RX_DR 6
#define BIT_TX_DS 5
#define BIT_MAX_RT 4
#define BIT_RX_P_NO 1
#define BIT_TX_FULL 0
#define BIT_PLOS_CNT 4
#define BIT_ARC_CNT 0
#define BIT_TX_REUSE 6
#define BIT_FIFO_FULL 5
#define BIT_TX_EMPTY 4
#define BIT_RX_FULL 1
#define BIT_RX_EMPTY 0
#define BIT_DPL_P5 5
#define BIT_DPL_P4 4
#define BIT_DPL_P3 3
#define BIT_DPL_P2 2
#define BIT_DPL_P1 1
#define BIT_DPL_P0 0
#define BIT_EN_DPL 2
#define BIT_EN_ACK_PAY 1
#define BIT_EN_DYN_ACK 0
/* Instruction Mnemonics */
#define CMD_R_REGISTER 0x00
#define CMD_W_REGISTER 0x20
#define CMD_REGISTER_MASK 0x1F
#define CMD_ACTIVATE 0x50
#define CMD_R_RX_PL_WID 0x60
#define CMD_R_RX_PAYLOAD 0x61
#define CMD_W_TX_PAYLOAD 0xA0
#define CMD_W_ACK_PAYLOAD 0xA8
#define CMD_FLUSH_TX 0xE1
#define CMD_FLUSH_RX 0xE2
#define CMD_REUSE_TX_PL 0xE3
#define CMD_NOP 0xFF
/* Non-P omissions */
#define LNA_HCURR 0
/* P model memory Map */
#define REG_RPD 0x09
/* P model bit Mnemonics */
#define RF_DR_LOW 5
#define RF_DR_HIGH 3
#define RF_PWR_LOW 1
#define RF_PWR_HIGH 2
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.