STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! State of GPIO after Watchdog Reset

Hello, I am using a STM32F401CE and would like to use the independent watchdog to cause a reset if the device would lock up for some reason. I have an external chip which is being controlled via GPIO and SPI from the STM32F401. When a watchdog rese...

JBlackann by Associate III
  • 1804 Views
  • 1 replies
  • 0 kudos

Hi Team, I'm using a STM32L4R5 and am wanting to store variables in SRAM2 as static variables so that they hold their value while the micro is in standby mode with SRAM2 retention enabled. What am I missing?

I've followed every tutorial/thread that i've been able to find but cannot get this to work. I've set: RAM2 (xrw) : ORIGIN = 0x20030000,  LENGTH = 64Kand .ram2_bss : { . = ALIGN(4); *(.ram2_bss) *(.ram2_bss*) } >RAM2In STM32L4R5ZITX_FLASH.ld and defi...

PLeij.1 by Associate II
  • 2420 Views
  • 5 replies
  • 0 kudos

SDIO 4 bit DMA UNKNOWN PROBLEM

This is sd_command line via logic analyzer. I'm writing 1024 bytes every second. But sd_commend do like that. And that's problem for me. If i wanna save some datas. sd_command line spoilng and locking my stm32f411 mcu's. I need help i don't understan...

0693W000007EhP0QAK.png
Vyagl.1 by Associate
  • 844 Views
  • 1 replies
  • 0 kudos

Hi ST Micro Would like to buy production qtys of STM32F205VET7 for 3 of my designs, cannot wait another year for delivery. Is this semiconductor still being produced OR do I need to re-design around it please. Scott_Davidson@Trimble.com

Suitable drop in replacements:STM32F205VET7   /original 512 KBytes flash, -40-105CSTM32F205VFT7   /768 KBytes flash, -40-105CSTM32F205VGT7   /1024KBytes flash, -40-105C

SDavi.2 by Associate
  • 929 Views
  • 1 replies
  • 0 kudos

Could not set IWDG timeout to max (~32s) for STM32G031?

I am using Nucleo-G031K board and attempt to set IWDG timeout to max value of ~32s. Got hard fault. Here is the code. Any idea?  iwdg_hIwdg.Instance = IWDG; iwdg_hIwdg.Init.Prescaler = IWDG_PRESCALER_256; iwdg_hIwdg.Init.Window = IWDG_WINDOW_DISABLE;...

Ccui.1 by Associate II
  • 3865 Views
  • 7 replies
  • 0 kudos

STM32F072RB in I2C slave mode

I am using STM as i2c slave. When other i2c master reads, first byte is always 0xFF and rest are correct data from STM with 1 byte shift so master needs to read 1 extra byte. Also I get HAL_I2C_ERROR_OVR error during that. Please suggest.

Multiprocessor mode with address mark detection only receives data which has '0' as MSB. After waking up (RWU=0) when the correct address is received subsequent bytes should be received normally, and not interpreted as another address?

I have configured the UART for multiprocessor communication over RS485. I can receive and transmit data correctly, but if the data contains a '1' as MSB it is interpreted as an address. Now it is clear from the documentation that this is the correct ...

0693W000007Ehc9QAC.png 0693W000007EhcsQAC.png 0693W000007EhgBQAS.png 0693W000007EhjoQAC.jpg
RWedu.1 by Associate II
  • 1064 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.