2021-02-10 1:43 PM
Hello,
I am using a STM32F401CE and would like to use the independent watchdog to cause a reset if the device would lock up for some reason. I have an external chip which is being controlled via GPIO and SPI from the STM32F401. When a watchdog reset occurs, does the GPIO outputs all default to Off? Is there I could keep an I/O line high (SET) over a Watchdog reset? I would like to not reset the external device if a watchdog event occurred.
Thanks.
Josh
Solved! Go to Solution.
2021-02-10 2:20 PM
Watchdog reset is like normal reset, setting all GPIO to default state. Only external pull cat set defined state.
2021-02-10 2:20 PM
Watchdog reset is like normal reset, setting all GPIO to default state. Only external pull cat set defined state.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.