STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to get an 8MHz sine wave HSE output on pin MCO1 (PA8) and should it be in phase with the original crystal signal?

I have been told i need to sync 2 STM32 MCU's together (on the same PCB) to stop an intermittent I2C bus failure between them. At the moment they are operating on separate 8Mhz crystals. I have used the following command to configure and output the 8...

Resolved! External interrupts on PC14 and PC15 of STM32F103C8T6.

Hello, guys.I need to improve one old project. There is no free pins on MCU left, except PC13-PC15 and I need three external interrupts. Code with initialization for making PC13-PC15 as inputs lower. I do not use LSE or RTC anyway.For PC13 all works ...

Antony1 by Associate II
  • 3239 Views
  • 4 replies
  • 0 kudos

TIM4 is a master, TIM3 is a slave. Given the same values I expected their respective CCx IRQ to fire at about the same time.

Set up TIM4 to generate a hsync pulse of 2us RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE); TIM_Cmd(TIM4, DISABLE); TIM_TimeBaseInitTypeDef timerInitStructure; timerInitStructure.TIM_Prescaler = 0; timerInitStructure.TIM_CounterMode = TIM_...

0693W000007YzcbQAC.png 0693W000007YzbZQAS.png 0693W000007YzclQAC.png

Resolved! Build server vendors (CI/CD) for STM32?

I'm looking for any potential vendors where I could host a cloud VM for doing automated STM32 builds coupled with some infrastructure for managing releases? Any recommendations?

AVoel.1 by Associate III
  • 2751 Views
  • 3 replies
  • 0 kudos

Custom loader internal & qspi possible?

Is it possible to write a custom loader (.stldr) for internal and external (qspi) flash? If so, any tips?I'm following this guide:https://www.st.com/content/st_com/en/support/learning/stm32-education/stm32-moocs/external_QSPI_loader.htmlThis is a tou...

Kvan .3 by Associate
  • 1194 Views
  • 2 replies
  • 0 kudos

Config of differential SDADCs in STM32F373

Hello all,I thought this is a straight forward thing but for me it turned out not to be...What I want to do is simply using SDADC1 and SDADC2 and perform a regular conversation at a time in multimode. I configured both in CubeMX and tried to sample b...

Bench by Associate III
  • 1459 Views
  • 2 replies
  • 1 kudos

Preprocessor Macro calculation

Hi, I have a question about preprocessor C. When I define macros like:#define CON_A 10 #define CON_B 5.6 #define CON_C 20.896 #define MY_MACRO (((10* CON_A)/CON_C)*CON_B)The last one is precalculated by the compiler or is just plain replaced as it...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.