2021-02-21 1:22 PM
Hi,
I am having some trouble with the CAN peripheral on the STM32F103C8Tx. I am using the HAL API's (via STM32CubeMX) to configure the device. I am using the device in loopback mode to test.
Up to now, I can successfully get the CAN peripheral to work in polling mode. However, I cannot for the life of me get the interrupt to fire for CAN_IT_RX_FIFO0_MSG_PENDING. Please see my code below, which I believe covers the correct setup procedure. I have also made sure to active the interrupt in the CubeMX setup.
//Initialise CAN
static void MX_CAN_Init(void)
{
/* USER CODE BEGIN CAN_Init 0 */
/* USER CODE END CAN_Init 0 */
/* USER CODE BEGIN CAN_Init 1 */
/* USER CODE END CAN_Init 1 */
hcan.Instance = CAN1;
hcan.Init.Prescaler = 4;
hcan.Init.Mode = CAN_MODE_LOOPBACK;
hcan.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan.Init.TimeSeg1 = CAN_BS1_15TQ;
hcan.Init.TimeSeg2 = CAN_BS2_2TQ;
hcan.Init.TimeTriggeredMode = DISABLE;
hcan.Init.AutoBusOff = DISABLE;
hcan.Init.AutoWakeUp = DISABLE;
hcan.Init.AutoRetransmission = ENABLE;
hcan.Init.ReceiveFifoLocked = DISABLE;
hcan.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CAN_Init 2 */
/* USER CODE END CAN_Init 2 */
}//Initialise filter
sf.FilterMaskIdHigh = 0x0000;
sf.FilterMaskIdLow = 0x0000;
sf.FilterFIFOAssignment = CAN_FILTER_FIFO0;
sf.FilterBank = 0;
sf.FilterMode = CAN_FILTERMODE_IDMASK;
sf.FilterScale = CAN_FILTERSCALE_32BIT;
sf.FilterActivation = CAN_FILTER_ENABLE;
if(HAL_CAN_ConfigFilter(&hcan, &sf) != HAL_OK)
{
Error_Handler();
}//Start CAN and activate interrupt
if(HAL_CAN_Start(&hcan) != HAL_OK)
{
Error_Handler();
}
if (HAL_CAN_ActivateNotification(&hcan, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
{
Error_Handler();
}//Transmit CAN data once every second (timer driven)
void CAN_Tx (void)
{
CAN_TxHeaderTypeDef TxHeader;
uint32_t TxMailbox;
uint8_t canMessage[8] = {0x02, 0x01, 0x0C, 0x55, 0x55, 0x55, 0x55, 0x55};
TxHeader.DLC = 8;
TxHeader.StdId = 0x7DF;
TxHeader.IDE = CAN_ID_STD;
TxHeader.RTR = CAN_RTR_DATA;
if (HAL_CAN_AddTxMessage(&hcan, &TxHeader, canMessage, &TxMailbox) != HAL_OK)
{
Error_Handler();
}
while(HAL_CAN_IsTxMessagePending(&hcan, TxMailbox));
}at this point I have the following call back function which resides in /* USER CODE BEGIN 4 */ ...
void HAL_CAN_RxFIFO0MsgPendingCallback (CAN_HandleTypeDef *hcan)
{
HAL_UART_Transmit(&huart2, (uint8_t *)"CAN_Received_OK\r\n", 17U, 100U);
}No matter what i try, I cannot get the callback function to be called.
I would be very grateful if someone could point me in the right direction,
Thanks in advance,
Richard.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.