STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Implications of underclocking HRTIM

Hi, I've got a bit of an odd question but I'm hoping someone will be able to help or at least point me in the direction of some further information.I am currently looking at a project where we need around 10 PWM outputs so we were looking at using th...

Gazmundo by Associate
  • 1233 Views
  • 1 replies
  • 0 kudos

SPI Slave NSS input not consistent

So I'm having this weird bug I can't seem to figure out.I'm trying to connect two stm32f4 discovery boards through SPI.The master is sending out a SS signal I want to use to synchronize with the slave.However for some reason before I send out a messa...

MDrac.1 by Associate III
  • 2908 Views
  • 2 replies
  • 0 kudos

hard fault when calling SBC_CleanDCache

I had some wrong bytes when transferring data over SPI, so I tried to clean the DCache. But I get a hard fault if I do this:I'm using the NUCLEO-H723ZG board.

0693W000008xqbnQAA.png
fb by Associate III
  • 1530 Views
  • 3 replies
  • 0 kudos

QSPI memory mapped mode reads 0xFFFFFFFF everywhere

Hi everyone,I have followed the tutorial from ST to set the external loader :https://www.youtube.com/watch?v=XqCq0xtQmbIhttps://github.com/STMicroelectronics/stm32-external-loader/tree/contribHere's my HW config :I use the same QSPI (MX25L51245G) tha...

0693W000008xPAaQAM.png 0693W000008xPAkQAM.png 0693W000008xPBEQA2.png

Hi all, I'm trying to configure my NUCLEO-H745ZI RAM as Device mass storage, i followed some tutoriels showing how to do this application with CubeMX and Keil IDE but its not working for me. I write my code only in "usbd_storage_if.c" file.

The code compile, load it to flash memory and enter debug mode to run the program.When i connect the usb connector present on the board to test if the computer will detect it as an usb device mass storage, nothing happen ! Can someone help with this ...

PyKe by Associate III
  • 1950 Views
  • 3 replies
  • 1 kudos

Unable to use PC14-OSC32-IN pin in NUCLEO-L152 Board

HI, i am new to STM32 controllers. i am using STM32L151RCT6 MCU in STM cube IDEJust i am trying to use PC14-OSC32_IN pin as input for external IRQ for falling edge configuration ..I not got the proper result , so just i configured that GPIO as input...

MBhir.11 by Associate III
  • 1222 Views
  • 1 replies
  • 0 kudos

Resolved! How to wake MCU from sleep by USART event

I'm learning STM32 by a NUCLEO-L053R8 board.  I want to put device to sleep (not LP Sleep, Stop or Standby) and wake it by either an interrupt or an event.int main() { // Clock and peripherals init // UART init (baud rate, GPIO, etc. are...

p80 by Associate II
  • 1482 Views
  • 1 replies
  • 0 kudos

How to measure the resources (run time / memory consumed) by having part of the code block in external memory encrypted (while using OTFDEC in L5 controller).

I am using STM32L562VE controller. I have configured OTFDEC with a portion of my code encrypted. Is there any way with which I can measure the run time and memory consumed promptly eventhough the code switches back and forth between internal flash an...

VNara.1 by Associate II
  • 866 Views
  • 0 replies
  • 0 kudos

Resolved! M95M02 eeprom Read And Write

Hello All ,I Am working On Interfacing M95M02 EEPROM With STM32 .Anyone Have Example Code for the same that is very helpful for me

Ajeth.11 by Associate III
  • 1896 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.