STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! no write access to ADC12_CCR registers of STM32G473QE

Hello,my problem is that i can't get access to the ADC12_CCR register. I activated the corresponding Clock in the RCC_AHB2ENR register. In addition I compare the addresses of the register from the library with the data of the reference manual, they a...

SMein.1 by Associate II
  • 1545 Views
  • 3 replies
  • 0 kudos

Resolved! PWM + DMA + 100% PWM duty bug, duplicated cycle

MCU: STM32F411CEU6.IDE: STM32CUBE IDE 1.5.1Timer1 config:PWM generation mode, CH1+CH2No prescaler, Period=549, Repetition counter = 8DMA: Circular mode, memory->periph, halfword, mem increase CH1+CH2PWM start code:// Ensure 32-bit alignment just in c...

0693W000008wriiQAA.png

How to protect my application code read from MCU?

I want to protect my code by writing OB using HALbool SetFlashReadProtection(bool state) { FLASH_OBProgramInitTypeDef OptionsBytesStruct = {0}; HAL_FLASHEx_OBGetConfig(&OptionsBytesStruct); if(state == true) { if(OptionsBytesStruct.RDP...

I am working for stm32h753zi and i am trying to measure ADC reference voltage. But i got 5.74466228 instead of 3.3v.Please any one give me the guidance. I have attached steps i followed, Thank you.

I am using the code :int read_adc_data(ADC_HandleTypeDef *ptr_hadc, uint32_t channelx){  uint16_t vrefint_cal;  float adc_read_value = 0.0, adc_reference_voltage = 0.0;  ADC_ChannelConfTypeDef sConfig;  sConfig.Channel    = ADC_CHANNEL_VREFINT;      ...

AFaya.1 by Associate III
  • 1698 Views
  • 4 replies
  • 0 kudos

The internal temperature measured by the ADC is different in debug and not debug mode. When I am debugging, the temperature value measured is correct (about 23°C). Without the j-link debugger, the temperature measured is incorrect (about 18 °C)

I send the temperature value on a serial interface.In the live watch of the IAR tool, I can see the same correct value than the one sent on the serial interface.The problem occurs after a power-down/power-up of my board, like if something is not init...

dlamb.1 by Associate II
  • 3612 Views
  • 8 replies
  • 0 kudos

Resolved! How to allocating dynamic memory in External SDRAM?

Hi all,I'm currently working on a project using the STM32H723 interface with SDRAM IS42S16400J. After booting up, I have to read a large JSON file [2MB] from flash into SDRAM then parse it to get the information. I wonder if I could allocating dynami...

Jumping to main program from ISR

Hi,I try to jump from Bootloader to my main program using this function:void jumpToMainProgram(){   uint32_t topOfStack = (*(uint32_t *)0x8008200ul);   HAL_RCC_DeInit(); // deinit clocks   // reset all periphals __HAL_RCC_AHB_FORCE_RESET(); __HA...

STM32F207+ADS127L01 SPI

Hi there i cant get a real data from ADS1227L01. In debug mode i see the value 0xFFFFFF.Q1: If anyone used ADS127L01 can they send me librarys for comparison ? Q2: Im using 3.75MBits/s Baund Rate is it enough for 24 bit data?

YCice.1 by Associate
  • 1135 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.