STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Generate a frequency burst

Hello,i try to implement a 40kHz frequency burst with my NULCEO STM32F411RE. Until now i toggle the GPIO continuously in the HAL_TIM_PWM_PulseFinishedCallback function. But now i have to implement a start Trigger to do a small 40kHz burst. In the att...

STM32F407 RTC skips a second on subsecond rollover

It appears that there is some unusual behaviour taking place when I read the time shadow register from the RTC. My application reads the RTC every 1000 systicks and prints the information.When the subsecond component rolls over to greater than the s...

TEgli.1 by Associate
  • 1577 Views
  • 1 replies
  • 0 kudos

Are the 6 fast channels on an STM32h742 ADC preconfigured by default as fast or I need to configure them as fast?

I have the package LQFP100, so the Application Note specifies that there are 3 fast channels, but the Reference Manual says that the first 6 input channels are fast channels. How is this? If I have to configure them as fast how can I do it or where c...

EEtxe.1 by Associate II
  • 665 Views
  • 0 replies
  • 0 kudos

IS STM32 chip producing now?

Now in China, all distributors don't have STM32F105RBT6, but if we ask from sub-distributors, most of them have massive in stock, just the price is very very high, about 14usd. So, please tell us when the supply can be normal, because if we switch ch...

VLiu.2 by Associate II
  • 1738 Views
  • 4 replies
  • 0 kudos

Resolved! How to reliably reset the microcomputer

MCU: STM32F769Thank you for helping.I may want to reset the microcontroller while the program is running.What kind of method is there to reliably reset the microcomputer in terms of software?Thank you.

Ebun.1 by Senior
  • 1400 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F410CBT3 사용해서 SPI를 통해 EXTERNAL MEMORY 컨트롤

현재 개발중�?� 시스템�? STM32F410CBT3 MCU를 사용하여 SPI를 통해 EXTERNAL MEMORY를 컨트롤 하고 싶습니다. �?�성파�?��?� 저장해야 �?�기때문�? 용량�?� 많�?� 차지 합니다.​SPI를 �?�용하여 EXTERNAL MEMORY를 사용할수 있는 방법�?�​회신주시기 바�?니다.​�?사합니다.​

GGIL.1 by Associate II
  • 1702 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.