2021-01-05 1:15 PM
I am looking for an expert to help me with I2C bus on STM32F407IGT. I2C3 is working as expected and I would like to make working also I2C1 and I2C2 which I have problems with.
I am using the same initialization regarding registers and I can see the right values on the right places (addresses) but I don't get any interrupt on I2C1 and I2C2. I set the start bit and a value in DR register but I can not see any clock or signal on pins. Any idea what to check?
Solved! Go to Solution.
2021-04-08 2:04 AM
Hi Amel
Thank you very much for your suggestion. Actually this was reason for I2C1 bus not working. After enabling the clock as a last step in initialization routine now I2C1 works as expected.
Regards
Simon
2021-01-05 2:21 PM
Check that the GPIO clocks are enabled and the pins are set to the correct AF mode. Check the I2Cx registers and compare the values for the working I2C3 and the not-working I2Cx. Check that the global interrupts for I2Cx are enabled.
2021-01-06 6:34 AM
Hi TDK
I have checked all registers which has something to do with I2C devices and I did not see any inconsistencies for I2C1, I2C2 compared to I2C3 which is working fine. Here is the printout of checked registers:
I2C1:
CR1 -> a=0x40005400: v=0x701
CR2 -> a=0x40005404: v=0x72a
OAR1 -> a=0x40005408: v=0x40a0
OAR2 -> a=0x4000540c: v=0x0
DR -> a=0x40005410: v=0x53
SR1 -> a=0x40005414: v=0x0
SR2 -> a=0x40005418: v=0x2
CCR -> a=0x4000541c: v=0xd2
TRISE -> a=0x40005420: v=0x2b
FLTR -> a=0x40005424: v=0x0
Using PB6->SCL, PB7->SDA:
MODER -> a=0x40020400: v=0x8284
OTYPER -> a=0x40020404: v=0x80
OSPEEDR -> a=0x40020408: v=0x80cc
PUPDR -> a=0x4002040c: v=0x104
IDR -> a=0x40020410: v=0x1cd8
ODR -> a=0x40020414: v=0x0
BSRR -> a=0x40020418: v=0x0
LCKR -> a=0x4002041c: v=0x0
AFRL -> a=0x40020420: v=0x44000000
AFRH -> a=0x40020424: v=0x0
I2C2:
CR1 -> a=0x40005800: v=0x501
CR2 -> a=0x40005804: v=0x72a
OAR1 -> a=0x40005808: v=0x40a0
OAR2 -> a=0x4000580c: v=0x0
DR -> a=0x40005810: v=0x35
SR1 -> a=0x40005814: v=0x0
SR2 -> a=0x40005818: v=0x2
CCR -> a=0x4000581c: v=0xd2
TRISE -> a=0x40005820: v=0x2b
FLTR -> a=0x40005824: v=0x0
Using PF1->SCL, PF0->SDA:
MODER -> a=0x40021400: v=0x140600a
OTYPER -> a=0x40021404: v=0x43
OSPEEDR -> a=0x40021408: v=0x3c0e00a
PUPDR -> a=0x4002140c: v=0x1404000
IDR -> a=0x40021410: v=0x8983
ODR -> a=0x40021414: v=0x8c0
BSRR -> a=0x40021418: v=0x0
LCKR -> a=0x4002141c: v=0x0
AFRL -> a=0x40021420: v=0x44
AFRH -> a=0x40021424: v=0x0
I2C3:
CR1 -> a=0x40005c00: v=0x1
CR2 -> a=0x40005c04: v=0x72a
OAR1 -> a=0x40005c08: v=0x40a0
OAR2 -> a=0x40005c0c: v=0x0
DR -> a=0x40005c10: v=0x97
SR1 -> a=0x40005c14: v=0x0
SR2 -> a=0x40005c18: v=0x0
CCR -> a=0x40005c1c: v=0xd2
TRISE -> a=0x40005c20: v=0x2b
FLTR -> a=0x40005c24: v=0x0
Using PH7->SCL, PH8->SDA:
MODER -> a=0x40021c00: v=0x29000
OTYPER -> a=0x40021c04: v=0x180
OSPEEDR -> a=0x40021c08: v=0x2b000
PUPDR -> a=0x40021c0c: v=0x1000
IDR -> a=0x40021c10: v=0x180
ODR -> a=0x40021c14: v=0x0
BSRR -> a=0x40021c18: v=0x0
LCKR -> a=0x40021c1c: v=0x0
AFRL -> a=0x40021c20: v=0x40000000
AFRH -> a=0x40021c24: v=0x4
RCC Registers:
CR -> a=0x40023800: v=0x3037283
PLLCFGR -> a=0x40023804: v=0x7405408
CFGR -> a=0x40023808: v=0x940a
CIR -> a=0x4002380c: v=0x0
AHB1RSTR -> a=0x40023810: v=0x0
AHB2RSTR -> a=0x40023814: v=0x0
AHB3RSTR -> a=0x40023818: v=0x0
APB1RSTR -> a=0x40023820: v=0x0
APB2RSTR -> a=0x40023824: v=0x0
AHB1ENR -> a=0x40023830: v=0x1011ff
AHB2ENR -> a=0x40023834: v=0x0
AHB3ENR -> a=0x40023838: v=0x0
APB1ENR -> a=0x40023840: v=0x10ea4030
APB2ENR -> a=0x40023844: v=0x24030
AHB1LPENR -> a=0x40023850: v=0x7e6791ff
AHB2LPENR -> a=0x40023854: v=0xf1
AHB3LPENR -> a=0x40023858: v=0x1
APB1LPENR -> a=0x40023860: v=0x36fec9ff
APB2LPENR -> a=0x40023864: v=0x75f33
BDCR -> a=0x40023870: v=0x0
CSR -> a=0x40023874: v=0x1e000000
SSCGR -> a=0x40023880: v=0x0
PLLI2SCFGR -> a=0x40023884: v=0x20003000
Where are global interrupt for I2C located? Maybe someone else can again check the registers, probably I did not seen something.
Best regards
Simon
2021-01-06 6:52 AM
> I have checked all registers which has something to do with I2C devices and I did not see any inconsistencies for I2C1, I2C2 compared to I2C3 which is working fine.
I2C1:
CR1 -> a=0x40005400: v=0x701
I2C2:
CR1 -> a=0x40005800: v=0x501
I2C3:
CR1 -> a=0x40005c00: v=0x1
These don't seem consistent to me.
2021-01-06 7:03 AM
This is an indication that I2C1 and 2 doesn't work that is why the bits are set. The question here is what to do to make I2C1 and 2 work. For this two ports I am setting start bit writing to DR reg every 100ms and for I2C1 also setting the stop bit. Just to see some action on the ports which does not happens. Pullup 10K is present on both ports. Is this the wrong procedure to get something send on ports?
2021-01-27 2:40 AM
Hi @SMali.3 ,
As you see in the I2C_SR2 register, the Busy bit is set for I2C1 & I2C2.
Make sure that the I2C pins are configured before enabling the I2C clock.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-04-08 2:04 AM
Hi Amel
Thank you very much for your suggestion. Actually this was reason for I2C1 bus not working. After enabling the clock as a last step in initialization routine now I2C1 works as expected.
Regards
Simon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.