STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How can I accept N IDs on CAN?

I'm trying to filter all IDs except 4 using the struct "FDCAN_FilterTypeDef", without using "FDCAN_FILTER_RANGE", "FDCAN_FILTER_MASK" but a type like "FDCAN_FILTER_DUAL" not with DUAL but N.How can implement it?

FScat.1 by Associate
  • 672 Views
  • 0 replies
  • 0 kudos

STM32 F4 - SDIO - Facing Data CRC failure while doing SDIO read/write, Anyway to avoid or recover this problem?

Hello!I am using STM32-NUCLEO-F412ZG board. I want to use SDIO (only IO) functionality as host.I am able to init, read, write to SDIO peripheral using polling.Before asking question let me give some background of implementation,Not using DMA4 bit SDI...

0693W000008ztvLQAQ.png
YMant.1 by Associate II
  • 1656 Views
  • 1 replies
  • 0 kudos

VREF+ Pin on STM32F103RCY6 (WLCSP64 Package)

I have a question regarding the VREF+ Pin in the above mentioned device. The datasheet DS5792 Rev 13 of the STM32F103xC devices states on page 36: " Unlike in the LQFP64 package, there is no PC3 in the WLCSP package. The VREF+ functionality is provid...

UART DMA TX

Hi there !Is the first time i wrote at this forum. I start to work with UART and DMA ,and i configurate the buffer in circular mode. I don't understa why when i call the library he continus to send over and over all i have in the buffer , i appearanc...

SGian.1 by Senior
  • 1558 Views
  • 3 replies
  • 0 kudos

Specifying the Interrupt priority.

Hi every body. I want to manage two events with general purpose timers 16 and 3. As a convention in ARM processors, as much as I know, the lower interrupt number corresponds to the higher priority. So I think I need to manage event with higher priori...

STork.1 by Associate III
  • 12164 Views
  • 1 replies
  • 0 kudos

STM32H743 AXI QOS

Hi,In RM0433 Reference Manual there is a description of the AXIM indicating the possibility to change the QoS for the AXI switch matrix, but cannot find the reference for the indexes used in AXI_INIx_READ_QOS or AXI_INIx_WRITE_QOS.If there any manual...

LGarc.2 by Associate
  • 2146 Views
  • 3 replies
  • 0 kudos

Resolved! My SPI clock produce 16bit rather than 8bit

I have a problem where my SPI clock produce 16bit, where I already set it to 8bit. I am not using any HAL driver, but I am learning from online course to develop my own driver from scratch.I have a problem at SPI master slave.The program is like this...

0693W00000900cfQAA.jpg
WM_IR by Senior
  • 1502 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.