STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H747 LDO power config

I'm trying to configure my custom board to only use the internal LDO, bypassing the need for the SMPS. In fact, my board doesn't even have the SMPS components. Is this allowed? The user manual seems to suggests that we can exclude the SMPS circuit ho...

0693W00000AMS4jQAH.jpg
TAtte.1 by Associate II
  • 1547 Views
  • 0 replies
  • 2 kudos

Hello! I am working on a project using the STM32H747 dualcore. The M4 core is responsible among other tasks for sampling a fairly quick digital signal (5-10 Mhz). I am looking for a hardware interface on the H7 that will allow me to sample this signal.

the sampling logic and countig is not very standard:1)     If A = rising edge and B = 0, counter++2)     If A = falling edge and B = 1, counter++3)     If B = rising edge and A = 1, counter++4)     If B = falling edge and A = 0, counter++5)     If A ...

yuri CH by Senior
  • 752 Views
  • 0 replies
  • 0 kudos

RXNE Flag of STM32F302R8 is never SET

Hi, I have a problem where my SPI SR RXNE in STM32F302R8 is never SET, causing my program always halt in while loop, waiting the RXNE status to become SET, when receive data.how I set the RXNE flag is below:#define SPI_SR_RXNE 0#define SPI_RXNE_FLAG...

WM_IR by Senior
  • 7044 Views
  • 11 replies
  • 1 kudos

Hai..., I am using STM32F746IGT custom boar QUADSPI W25Q128A and custom External Loader CLIVEONE "Stldr" file for PF7,PB6,PB2,PF9,PF8,PF6 PIn configuration , When i go to Debug mode geting error.

Erasing memory corresponding to segment 0:Erasing internal memory sectors [0 4]Error: failed to erase memoryError: failed to erase memoryEncountered Error when opening C:\ST\STM32CubeIDE_1.6.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltoo...

GMano.1 by Associate II
  • 1021 Views
  • 1 replies
  • 0 kudos

Can't start first code with NUCLEO-H755ZI-Q

I bought a new NUCLEO-H755ZI-Q board. It's my first STM32. I use MXCube to create a new project for MDK-ARM. I tried both STM32H755ZI and Nucleo-H755ZU-Q. And I enter my code in Application/User/CM7/Core/main.c . Between line 163 "/* USER CODE BEGIN ...

JZhan.15 by Associate
  • 3069 Views
  • 4 replies
  • 0 kudos

Resolved! In input capture function , i am trying to interface HC-sr04 Ultrasonic sensor to STM32F401. I am giving input to TRIG pin with 10 micro seconds ON and Need to Measure Pulse from ECHO pin of the Sensor and not getting Exact Width.

The Pulse width value of the waveform in input capture is not matching with orginal Pulse from sensor output .Please help.#include<NEW.h>#include<stdio.h>#include<stdarg.h>void Ultra_setting();void delay(int val);void Tim3_Capture();void Uart1_config...

0693W00000AMQ1dQAH.png 0693W00000AMQ1YQAX.png
Nchun.1 by Senior
  • 2860 Views
  • 2 replies
  • 0 kudos

Resolved! How to enable Capture/Compare 1 output Polarity(11: noninverted/both edges) in TIMx_CCER Register(STM32F401RE) but only 1 Bit is allocated for CC1P?

In detail glance on RM0368 Reference manual. I am getting confused while enablingCC1P -Capture/Compare 1 output Polarity(11: noninverted/both edges) in TIMx_CCER Register(STM32F401RE) .Whether it is possible to change Output Polarity into both Risi...

0693W00000AMOeOQAX.png 0693W00000AMOeYQAX.png
Nchun.1 by Senior
  • 1913 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H743 5V tolerant pins for an LQFP176 Package

Hello, I have a doubt about the voltage tolerance of STM32H743: looking at Stm32h743bi.pdf, LQFP176 pins are numbered 1,2,...,176, while CubeIDE gives me PA1, PA2, PB1, PB2.... etc.So, how can know if my UART3 pins (PB10 & PB11, Alternate function P...

Resolved! Hello everyone, I have to implement SMBus communication with battery. I read X-CUBE-SMBUS Software is only compatible with NUCLEO-G431RB, NUCLEOH743ZI, NUCLEO-L4R5ZI, 32F072BDISCOVERY, 32L0538DISCOVERY, 32L476GDISCOVERY, and STM32F3DISCOVERY boards.

I have an STM32 F401RE (NUCLEO - 64)board. In the document " Description of STM32F4 HAL and low-layer drivers" there are HAL SMBUS Generic drivers. Is it possible to implement SMbus communication using this board or I will have to purchase on of the ...

Shubham1 by Associate
  • 2225 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.