2021-04-28 1:49 PM
The RM0444 Rev5 show 36 EXTI lines in Table 62.
The HAL code defines up to 37 lines:
/**
* @brief EXTI Line number
*/
#if defined(STM32G0C1xx) || defined(STM32G0B1xx)
#define EXTI_LINE_NB 37uL
#elif defined(STM32G0B0xx)
#define EXTI_LINE_NB 37uL
#elif defined(STM32G081xx) || defined(STM32G071xx)
#define EXTI_LINE_NB 34uL
#elif defined(STM32G070xx)
#define EXTI_LINE_NB 34uL
#elif defined(STM32G041xx) || defined(STM32G031xx)
#define EXTI_LINE_NB 32uL
#else
#define EXTI_LINE_NB 32uL
#endifWhere can I found some info on the missing line ?
Another question:
Where can I found a table with the correspondences between the EXTI lines numbers and the interrupt numbers?
There is only some lines documented in the NVIC chapter.
I am particularly looking for EXTI 20, 29, 30, 31, 35, 36
Thank you
2021-04-28 2:34 PM
The direct events do not have an associated EXTI interrupt. The EXTI only wakes up the system and CPU sub-system clocks and may generate a CPU wakeup event. The peripheral synchronous interrupt, associated with the direct wakeup event wakes up the CPU.
Pretty sure the ones you cite are flagged as "DIRECT" in the EXTI section
The NB is presumably 0 thru 36, being 37 in number
2021-04-28 3:06 PM
What mean these lines in stm32g071xx.h:
I2C1_IRQn = 23, /*!< I2C1 Interrupt (combined with EXTI 23) */
USART3_4_LPUART1_IRQn = 29, /*!< USART3, USART4 and LPUART1 globlal Interrupts (combined with EXTI 28) */
CEC_IRQn = 30 /*!< CEC Interrupt(combined with EXTI 27) *EXTI 23, 28, 27 are Direct, but mentioned in the IRQ list. What mean "combined with EXTI" ?
The RM lists EXTI from 0 to 35, so 36 EXTI lines. The AHL defines 0 to 36 => 37 EXTI lines...
#if defined(LPUART2)
#define EXTI_LINE_35 (EXTI_DIRECT | EXTI_REG2 | 0x03u)
#else
#define EXTI_LINE_35 (EXTI_RESERVED | EXTI_REG2 | 0x03u)
#endif
#if defined(STM32G0C1xx) || defined(STM32G0B1xx) || defined(STM32G0B0xx)
#define EXTI_LINE_36 (EXTI_DIRECT | EXTI_REG2 | 0x04u)
#endifThe RM0444 is for STM32G0x1, so it is also for STM32G0C1xx
2021-04-28 3:31 PM
>>What mean "combined with EXTI" ?
That the IRQ Handler is invoked if the PERIPHERAL or the EXTI signal (figure an AND or OR gate depending on the normal state of those pins/signals)
Half expect COMP3 (which has sketchy coverage in the RM) to dump out to ADC1_COMP_IRQHandler
Perhaps
29 LPTIM1 TIM6_DAC_LPTIM1_IRQHandler
30 LPTIM2 TIM7_LPTIM2_IRQHandler
Yeah, the docs/source is pretty horrific.. one of those cases where ST seem to comingle several IC die into one Reference Manual
and that the CM0(+) has very limited NVIC
@Imen DAHMEN
2021-04-29 3:36 AM
Hello,
Thanks @Nikita91 and @Community member for pointing out this issue.
I will check this and take the necessary action for fix.
Imen
2021-04-30 2:16 AM
It seems that USB wakeup line is in RM. I raised your feedback to the Doc Owner to fix this in the coming RM revisions.
Thanks for noticing it.
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.