STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4R5 Quadrature Encoder Hardware Connection

I'm trying to connect a quadrature encoder to my board using STM32L4R5. From what I understand, I should connect the A and B to TIM2, TIM3, TIM4 or TIM5. If I have 2 encoders, can I connect all 4 A and B signals from both encoders to the same TIM? Li...

CYeow.1 by Associate II
  • 1362 Views
  • 2 replies
  • 0 kudos

Resolved! Can't enable DMA stream for UART4 Tx

Currently I am using the STM32H753ZIT6 to do all the bare metals. Essentially what I am trying to do is just enable UART4 Tx to send some debug messages thats all. Everytime I try to enable the DMA1_Stream3 (UART4_Tx) it just gives me a TEIF3 error a...

CLeo.1 by Senior II
  • 2823 Views
  • 7 replies
  • 0 kudos

5V-tolerant input pulls 5V down to 4V

Hi all:I am using an STM32407 running at 3.3V, and I have 2 inputs connected to 5V signals.One of the signals comes from an outside sensor (a data line), and the other one is connected to a 5V optocoupler populated on the same board.I have measured t...

Diez.R. by Associate II
  • 4884 Views
  • 8 replies
  • 0 kudos

Resolved! State of UART pins during a reset on STM32F439

I am having a hard time finding out the state of the UART pins while the chip is held in RESET. Are pins E2, D5, D4, and E1 held in a high-impedance state while the RESET pin H9 is pulled low? I suspect they are, but am trying to confirm through docu...

LKish.1 by Associate
  • 2766 Views
  • 3 replies
  • 0 kudos

I2C stm32F103

Hi,i come up with my question related to I2C communication using stm32F103,I would like to interface my I2C LCD (slave) with MCU ( master), but i have a problem with the Transmit sequencei have configured the GPIO's PB6 (SCL) and PB7(SDA) as open dra...

0693W00000ANH9uQAH.png
SIDRI.1 by Associate III
  • 1456 Views
  • 0 replies
  • 0 kudos

digital clock in custom container

Hi, I have a custom container that includes a digital clock. But when I set the clock any initial time, it starts from 00:00:00. How do I set the clock to the initial time that I want?

Ezgi by Senior
  • 928 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.