2021-05-04 1:00 AM
Hello,
i´m working with a STM32H743ZIT and have a problem with the initialization of ADC with DMA.
Only ADC1 with DMA is OK
Only ADC2 with DMA is OK
Init ADC1 und ADC2 with DMA fail.
Is this problem known?
Thanks for help and regards
2021-05-04 2:04 AM
Hi @MHiep.1
You can refer to ADC_DMA_Transfer example provided in STM32CubeH7 firmware via this path: STM32Cube\Repository\STM32Cube_FW_H7_V1.8.0\Projects\STM32H743I-EVAL\Examples\ADC\ADC_DMA_Transfer
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.