STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

complementary PWM I want to create the complementary PWM pulses in timers, for pulses with a specific dead time.

I actually need 6 Plus. (3 pulses (not) are other pulses). I have generated 4 pulses with two timers 1 and 8 and I need to generate two more pulses, but I can not produce dead time with advanced timers. I have used advanced timers and I need to have ...

amir_pdn by Associate II
  • 2895 Views
  • 5 replies
  • 0 kudos

Resolved! Can VREF+ be zero?

In STM32F437 data sheet it says VDDA - VREF+ < 1.2 V.Is that a "global" limitation or just a working limitation?If VDDA is 3.3V and VREF+ is 0V, can that harm the chip, or is it just that the conversions don't work right?

Problem with code slowness

Hi all,​I am using the Delay​ function as follows.static void Delay(volatile int d) {  d = d*20;  while (d--) asm volatile("NOP"); }​​However, sometimes when adding printf code, Delay function becomes slow.So, when I analyzed the cause, I was able to...

sim20 by Associate II
  • 1086 Views
  • 1 replies
  • 0 kudos

Utilize SDRAM on STM32H743 EVAL2 Board

I'm having trouble making use of SDRAM (external device memory) on the STM32H743 EVAL2 board. Specifically, I'm trying to make use of FMC SDRAM Bank 2 (Region: External Devices) to store a large array. Here are code snippets that I have added/modifi...

0693W00000BaKybQAF.png
matt12345 by Associate II
  • 6761 Views
  • 7 replies
  • 0 kudos

STM32L412 UART bootloader not writing data

Hi, I'm curentlly in the process of switching to a STM32L412 from an STM32F3 on a custom design and I'm having an issue with the UART bootloader. The bootloader worked as intended on the F3 chip but on the L4 chip I can't write to the chip. Everythin...

fabces by Associate
  • 1185 Views
  • 1 replies
  • 0 kudos

Resolved! How to add fsdata.c file to project?

Posted on March 19, 2017 at 21:42I have the STM32F407 Discovery board running with LWIP. I am able to ping the board and get replies.I now want to get a Web Server running on the board. I used CubeMX and Enabled LWIP_HTTPD on the HTTPD configuration...

STM32F4 Custom board HID device

Hello. I am developing a custom board with STM32F405. I want it to work as custom HID device. The board must connect to the PC through an already existent driver software. I tested he board with the Keyboard and Custom HID device examples in the pack...

VCapu by Associate III
  • 2698 Views
  • 4 replies
  • 0 kudos

how to use osMessageQueueNew

hello,I am using ADC for data acquisition using 46 uSec. I would like to do some calculation every 4 samples. I am using timer to trigger Adc reading. Can I use osMessageQueue in ADC complete conversion call back function to put 4 new adc reading int...

yang hong by Associate III
  • 1420 Views
  • 0 replies
  • 0 kudos

Resolved! SPI signal looks weird on STM32F746

Hi,I have a custom board with STM32F746 MCU and XPT2046 touch controller (Clone of TI TSC2046E). They are connected on SPI2 (no other devices on this bus), running at ~210Kbit/s.I couldn't get the touch controller to work correctly, so I've connected...

RZahor by Associate II
  • 2852 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.