STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hello to everyone, I just joined the Stm32 family and I chose the STM32F373C8T6 chip to use in my projects. The reason I chose this mcu was that I used two different SPI communication components in the project I wanted to do.

Hello to everyone,I just joined the Stm32 family and I chose the STM32F373C8T6 chip to use in my projects. The reason I chose this mcu was that I used two different SPI communication components in the project I wanted to do. But since I am very new, ...

RŞahi.1 by Associate II
  • 1177 Views
  • 1 replies
  • 0 kudos

Memory malloc fails after upgrading of new firmware.

Hello @Martin KJELDSEN​ @All ALL​ ,Facing issue in up-gradation of new firmware in following scenarios.I am using "STM32F412CGU6" microcontroller with MPU protection.My application stores the new firmware in an external SPI flash. Firmware data recei...

Resolved! Having problem with I2C4 in stm32H747 Disco

I am using STM32H747I-DISCO discovery kit. I want to use I2C4 in the kit but clock is not generated in scl. I am using pin D15 as SCL and pin D14 as SDA of CN5 connector of discovery board. According to the user manual of discovery board D15 is conn...

SLuit.1 by Associate III
  • 2186 Views
  • 2 replies
  • 0 kudos

I2C communication halted in HAL_GPIO_EXTI_Falling_Callback

I'm a biginner on embedded programing and facing an I2C communication halt issue when I put HAL_I2C_Master_Seq_Transmit_IT() in HAL_GPIO_EXTI_Falling_Callback(). STM32CubeIDE: Version: 1.6.0, Build: 9614_20210223_1703 (UTC)Target board: NUCLEO-G031...

MMish.2 by Associate
  • 1675 Views
  • 2 replies
  • 0 kudos

Sigma-Delta ADC STM32F373 calibration problem

Hi,I have connected three channels of the SDADC in the STM32F373 with an external voltage reference of 1.225V. The selected mode of the ADC is Single-ended zero-volt reference mode, and i am reading these channels using the "injected conversion" as i...

DCajigal by Associate III
  • 5234 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.