2017-03-19 1:42 PM
I have the STM32F407 Discovery board running with LWIP. I am able to ping the board and get replies.
I now want to get a Web Server running on the board. I used CubeMX and Enabled LWIP_HTTPD on the HTTPD configuration tab. I generated the code and imported it into System Workbench.
I created a simple web page with two html files. I then used makefsdata.exe to create the fsdata.c file and added it to the project.
When I compile the project, I get these errors:
Middlewares/Third_Party/LwIP/src/apps/httpd/fsdata.o:(.rodata+0x0): multiple definition of `file__related_html'Middlewares/Third_Party/LwIP/src/apps/httpd/fs.o:(.rodata+0x0): first defined hereMiddlewares/Third_Party/LwIP/src/apps/httpd/fsdata.o:(.rodata+0x14): multiple definition of `file__programming_html'Middlewares/Third_Party/LwIP/src/apps/httpd/fs.o:C:\STMNew\Eth-Test\Release/../Middlewares/Third_Party/LwIP/src/apps/httpd/fs.c:85: first defined hereI looked in fs.c and do not see my two html files (related.html, programming.html) mentioned anywhere so I don't understand why the linker thinks there are multiple definitions.
I believe the errors may be related to this code in fs.c:
#if HTTPD_USE_CUSTOM_FSDATA#include 'fsdata_custom.c'#else /* HTTPD_USE_CUSTOM_FSDATA */#include 'fsdata.c'#endif /* HTTPD_USE_CUSTOM_FSDATA */Is there a document available that has instructions on how to setup a Web Server using System Workbench? I've searched but haven't really turned up any useful information. I do find some
stuff for LWIP v1.0.1. But I assume System Workbench is using some variation of v2.x.x
Solved! Go to Solution.
2017-03-29 8:12 AM
Hello,
as you can see in fs.c file, fsdata.c is directly included at the begining of fs.c, so it means that the compiler physically copy the content of fsdata.c file at the place of #include 'fsdata.c' directive and then compile the whole file.
So to fix multiple definition you need to exclude fsdata.c from your project build (for exemple if you use eclipse, right click on the file, select Properties and check 'Exclude from build')
Hope it will help you
2017-03-21 8:12 AM
same issue here. I'm not able to run webserver example on ac6 ide because 'multiple definition error' on fs.c
2017-03-29 8:12 AM
Hello,
as you can see in fs.c file, fsdata.c is directly included at the begining of fs.c, so it means that the compiler physically copy the content of fsdata.c file at the place of #include 'fsdata.c' directive and then compile the whole file.
So to fix multiple definition you need to exclude fsdata.c from your project build (for exemple if you use eclipse, right click on the file, select Properties and check 'Exclude from build')
Hope it will help you
2017-03-29 2:28 PM
Yes, someone else pointed that out. Once I excluded the fsdata.c file from the project build, I was able to successfully compile the code. Everything is working fine now. I have a temporary webpage being displayed. I haven't gotten around to setting up a page so I can have callback functions to test yet. Hopefully I will get to that in the next week or so.
2017-10-19 12:35 AM
Where should the fsdata_custom.c be located? It works fine in the httpd directory however it is deleted by CubeMX with a new project generation. Logical should be be Src together with the other custom files. This gives an error: fc.c cannot find fsdata_custom. My Src is included in the Source locations. Or should i place is somewhere out of reach so 'exclude from build' is not needed?
2019-07-28 4:17 AM
Hello,
I have same problem... I must manually recopy file on each code regeneration ???
Any solution ?
Regards,
Bully.
2020-03-30 2:35 AM
Did you ever get a solution to this problem? I'm having it right now. Thanks
2020-03-30 10:22 AM
Yes, place fsdata_custom.c in Middlewares/Third_Party/LwIP/src/apps/http. The latest version of CubeMX for some stupid reason wants to see the file in that directory. I don't know what http has to do with httpd but maybe the programmers at ST had a reason to think they were related. The older versions of CubeMX had it correctly placed in the httpd directory. Each regeneration of the code will remove the file so save a copy so you can copy it back to the http directory.
2021-06-07 2:14 PM
Old thread, but for this specific reason I have just added the ../Src directory to the include directories, allowing me to place fsdata_custom.c in the normal Src directory. Not the "neatest" solution but as long as you don't misuse it for anything else, it's a clean enough solution for now and you can just regenerate.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.