STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! identifie counterfeit

Hello,we had trouble with a batch of STM32F103CBT7 processors. I have read a lot about counterfeit CPU's. I had the Error 18 in CubeIDE and 5 out of 1000 IC's did not work as our stock ones (STM32F103CBT6). The UID of one of the chips is UID0= 0x0047...

machinist by Associate III
  • 3250 Views
  • 4 replies
  • 0 kudos

How to Solve the default handler ISR . In my code PC struck in default handler function in startup_stm32l476xx.s file

Hi,In my code Program counter struck in Default hander routine.  .section .text.Default_Handler,"ax",%progbitsDefault_Handler:Infinite_Loop: b Infinite_Loop .size Default_Handler, .-Default_Handler how to know what is the cause for this and how to o...

Skuma.12 by Associate II
  • 931 Views
  • 0 replies
  • 0 kudos

Debug the application from external memory interface.

hi we want to debug from the external memory interface. Actually my code size is more than internal RAM memory, so we want use external memory jtag debugging. is this external memory debugging possible? if possible what is procedure ?

srikanth by Associate III
  • 2021 Views
  • 6 replies
  • 0 kudos

USART IDLE Line Interrupt

I have an idle interrupt, on usart2 handle;void USART2_IRQHandler(void)   {   /* USER CODE BEGIN USART2_IRQn 0 */   /* UART IDLE Interrupt */   if(__HAL_UART_GET_FLAG(&huart2, UART_FLAG_IDLE) == SET)   {   __HAL_UART_CLEAR_IDLEFLAG(&hu...

DCtech by Associate II
  • 6787 Views
  • 11 replies
  • 0 kudos

Interrupt Latency Measurement

Hello,I have three interrupts,One from EXTI4, which has NVIC_IRQChannelPreemptionPriority = 0One from EXTI9_5 which has NVIC_IRQChannelPreemptionPriority = 1One from TIM4 which has NVIC_IRQChannelPreemptionPriority = 2For testing purposes, EXTI4 and ...

JTone.1 by Associate
  • 2075 Views
  • 2 replies
  • 0 kudos

DMA - Normal vs Circular

Hello, what's the difference between the "Normal" and "Circular" modes of the STM32 DMA ?As far as I understand - "Circular" will write to the first address, auto increment the address to the next one until the last address is reached and then return...

skon.1 by Senior
  • 22496 Views
  • 5 replies
  • 3 kudos

Hello, I am using stm32f407vgt6 that supports fsmc, I need to extend the RAM; is it possible to interface hyperbus RAM chips using the FSMC? if not what are the possible alternatives? kinly note stm32f407vgt does not support QSPI.

Hyperbus RAMs requires 12 pins for implementation and offer decent speed. I have already 16 spare pins for the data/address and 10 other pins for fsmc handshaking. have any one tested this option before? is this easily implemented using HAL library o...

JAbde.1 by Associate
  • 740 Views
  • 0 replies
  • 0 kudos

Sharing flash sector when using dual-bank mode.

Hi,I'm using the flash in a dual-bank mode. I would like to have a common (shared) sector between the 2 banks for storing configuration data. This becomes somewhat tricky when addresses are shifting according to the active bank. How should I go about...

Eitan by Associate
  • 1248 Views
  • 1 replies
  • 0 kudos

What's the macro for NUCLEO-G474RE?

I tried this tutorial - https://www.carminenoviello.com/2015/06/04/stm32-applications-eclipse-gcc-stcube/ - Build STM32 applications with Eclipse, GCC and STM32Cube. In the last,it was said:we have to declare which MCU we are using defining a global ...

MQi.1 by Senior II
  • 1060 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.