2021-06-28 5:32 PM
안녕하세요.
기존�? 사용중�?� 시스템 (PIC 계열) �?서 MCU 만 �?체를 하여 사용�?� 하려고 합니다.
기본 Digital I/O 신호가 5V �?��?�요.
STM32F405RG �?� Datasheet 를 보면서 �?금�?�?� 있어 문�?�를 드립니다.
I/O structure 가 FT �?� 경우, 기존 사용하면 신호를 그대로 연결�?� 해�?� 무방한지요?
아니면 Level shift 회로를 추가하는게 좋�?�지요?
2021-06-30 8:27 AM
Hi @CJeon.1 ,
First of all, welcome to ST Community!
As the common used language in this community is English, I tried to translate your question and I got this result:
*****************************************************
STM32F405RG series inquiry
Good morning.
I want to use it by replacing only the MCU in the existing system (PIC series).
The basic digital I/O signal is 5V.
I have a question while looking at the datasheet of STM32F405RG, so please inquire
If the I/O structure is FT, is it okay to connect the signal as it is if it is used in the past?
Or is it better to add a level shift circuit?
*****************************************************
I am not sure to fully understand it based on this translation. So please explain it more.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.