2021-08-13 6:03 AM
I've clear (or at least I think so) how to use the timers (TIM), with "Input capture direct mode", in order to measure a period of one input pulse, but I don't understand how to do the same measure with the low power timer (LPTIM). The LPTIM associated with an external source seems dedicated to counting events.
I need one (o more) example, but all I found is TIM-related.
Can I have any help?
Grazie.
F.
2021-08-15 3:09 AM
Unfortunately, LPTIM is not equipped with input capture nor similar mechanism, so you cannot measure period of a signal.
JW
2021-08-16 2:18 PM
Ma che tristezza. :(
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.