STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4S9 SAI Configuration Full Duplex

Hi,I would like to use the SAI as full duplex slave mode with I2S/PCM protocol.I'm not sure about the configuration and which pins are TX and RX when using Cube. In the parameter I can set the audio to transmit or receive.In this case SAI_SD_A will b...

0693W00000DqI2kQAF.png 0693W00000DqI5AQAV.png
NKara.3 by Associate II
  • 1255 Views
  • 1 replies
  • 0 kudos

SWD connexion for custom board

I have an ST link V2 and a custom board running at 3.3V generated by an on-board regulator powered from a battery. Google is sending me mixed messages about connecting VAPP (pins 1 and 2) on the ST link to VDD on the board. I'm a bit worried about de...

DCarr.1 by Senior
  • 1330 Views
  • 3 replies
  • 0 kudos

Resolved! two UART DMA with timer interrupt

Hi, allI am trying to receive packet from uart3 and send them to uart2but the results of my trials are:transmit occurs every main cpu clocktransmit occur just oncewhich I thought was:receive packet from uart3 when packet arrived, independentlytransmi...

Frogram by Associate II
  • 3458 Views
  • 5 replies
  • 1 kudos

Need to change interrupt priority for USART DMA RX Circular

I've got some code working from an example for USART RX DMA Circular. I'm to the point where I can receive the UART data but I need to now use a write to a protected (by a binary semaphore) circular buffer from the interrupt context HAL_UARTEx_RxEve...

ATzou.1 by Associate II
  • 8110 Views
  • 11 replies
  • 0 kudos

No while loop shown in tutorials in main.c

Hi,I've seen that in many stm32 tutorials (such as blinking LED and uart tutorials) they make use of a "while (1) " loop located in main.c:  But, in the main.c generated by cubeMX for my stm32l496ag board i have only the following single while loop, ...

0693W00000Dq5C4QAJ.png 0693W00000Dq5KHQAZ.png
CHech.1 by Associate III
  • 1512 Views
  • 2 replies
  • 0 kudos

STM32F401VET6 flash partition to store 3 binary files at particular flash addresses. These binary files need to be used for some product applications.

We have STM32F401VET6 in our product development. Currently, our project (makefile) compiles and stores application binary in STM MCU internal flash. We would like to store three other binary/hex files to the STM MCU internal flash as part of the bui...

0693W00000DqGkvQAF.jpg
JSaro.1 by Associate II
  • 3995 Views
  • 9 replies
  • 0 kudos

Retrieving multiple SPI packets from DMA

Hi guys I have set up my STM32 as an SPI full duplex slave device. All SPI communication happens through DMA. The Master device is a Beaglebone Black communicating over linux spidev driver. The problem I am facing now is if the master sends multiple ...

SDas.1 by Associate II
  • 2751 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.