STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Error in CAN transmission normal mode

I am using 2 microcontrollers STM32F103ZETx as transmitter and STM32F730R8 as reciever. So my CAN is coming into initialization mode but has some issues in CAN normal mode. SLAK=0 , INAK=1(should be 0) and INRQ = 1(should be 0) for can normal mode.1....

SMitt.2 by Associate II
  • 2950 Views
  • 3 replies
  • 0 kudos

VCP with STM32F429I DISCO

I don't understand why i can't use VCP on my STM32F429I-DISCO even if UART RX /TX pin are connected to the USB-ST-link. I know I have to flash this ST-link V2 to V2.1 to have the VCP activated but i can't do that.You can see on the attached schematic...

0693W00000FACvJQAX.png
doddonny by Associate II
  • 1758 Views
  • 2 replies
  • 0 kudos

STM32 I2C Slave mode HAL bug

Recently I have tried to implement a solution employing I2C interface in slave mode.The solution follows the pattern presented in the official I2C_TwoBoards_RestartAdvComIT example available in CubeMX packages and another solution presented here: STM...

TDJ by Lead
  • 2767 Views
  • 2 replies
  • 1 kudos

FMC/FSMC ECC computation

Hello, guys!I have a quick question about FSMC's ECC routine.From what I understood, the workflow goes like this:1) Enable ECC computationSET_BIT(hnand->Instance->PCR, FMC_PCR_ECCEN);2) Write data to the target device3) Get the computed ECCwhile (__F...

PMera.1 by Associate III
  • 1837 Views
  • 2 replies
  • 0 kudos

STM32F7 SMBUS vs STM32F4 SMBUS

Differences in setting up for SMBUS:On F4, I set the following bits in CR1: PEC POS ENPEC SMBTYPE SMBUSOn F7, are there similar bits?I see PECEN - is that the same as ENPEC on F4?How do you set up SMBUS on F7? (on F4, it was done with SMBTYPE and SMB...

TAnde.5 by Associate II
  • 889 Views
  • 0 replies
  • 0 kudos

Resolved! ADC noise on stm32f401

I've been messing around with a LMT86 temperature sensorThis sensor is deemed high output impedance as the documented loads it drives is 50uA.ADC noise on STM32 isn't 'new'. Just that for a first time I'm observing such volatility up close. The probl...

0693W00000Dnmj4QAB.png 0693W00000DnmjsQAB.png 0693W00000DnmlPQAR.png 0693W00000DnmmwQAB.png
andrewg by Associate III
  • 11109 Views
  • 16 replies
  • 0 kudos

stm32f429 shortage

Hello everyone ; I dont know if this is the right place to write ; we are using stm32f429 in our products we use about 20K / year . we are doing the plan for the next year we are getting a long ..very long shippng dates like 80 weeks ! even now we...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.