2021-09-22 11:25 PM
2021-09-22 11:54 PM
Welcome, @Kh.2, to the community!
I've translated your question using a translation tool to increase the chances of getting you a reply from our experts and community members, since the majority interact in English.
Here is the translation of your post using Google translate:
How to unlock the STM32G031C8 chip after it is read protected?
That depends on which RDP level (Read Protection) is active: Level 2 is a one-way street and can no longer be unlocked. On the other hand, level 1 can be changed to level 0, details can be found in RM0444, section 3.5.1.
Google translates the answer to: 这�?�决于哪个 RDP 级别(读�?��?护)处于活动状�?:级别 2 是�?��?�街�?�,无法�?解�?。 �?�一方�?�,级别 1 �?�以更改为级别 0,详细信�?��?�以在 RM0444,第 3.5.1 节中找到。
Good luck!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.