2021-09-27 10:13 AM
For example, if I send 1000, it will be received as 0100 on the STM board. I send what I received in the Rxcallback function. My program doesn't work, so I know this is the case. This issue stops after I hit the RESET switch on my board. Now, my issue is that for my university project, the STM board is locked in a box. It can't be reset. So how do I fix this issue in software, if possible? Or will I have to do some soldering...
The CubeIDE also does the same thing when debugging, it restarts the board after the initial connection to it. Is it because I was debugging it beforehand? The UART is in async mode so it should not need any clock synchronization, but are there any stop/begin specific characters in stm32, I haven't heard of such a thing.
2021-09-27 10:44 AM
> For example, if I send 1000, it will be received as 0100 on the STM board.
There's nothing on the STM32G4 that is going to transpose the first two characters. Most likely there is a bug in your software, or the data on the line isn't what you expect, perhaps due to the terminal program buffering data. Do you have pullups on the RX line? What exactly are the hardware connections?
Also likely is that your receive calls are out of sync with what's being sent, so you're getting the end of one transmission, plus the start of another.
2021-09-27 10:59 AM
Does your "protocol" have any sync mechanism, incase there is some noise on startup/powerup?
Typically for console user input a CR Carriage return terminates one input, and preps for next (or an LF, or a CRLF sequence).
Maybe set your code to expect a CR before the 1000, and expect a CR to terminate the 1000 (as when you type on a keyboard to a PC console). i.e. idle waiting for a CR, then print a prompt asking for the input value.
Paul
2021-09-27 12:09 PM
I'm using a micro-USB cable to connect to my PC via USB. In the .ioc file of my program the 2 pins (RX/TX) for the LPUART have the following settings:
GPIO Mode; Alternate Function Push Pull
GPIO Pull-up/Pull down; No pull-up and no pull-down
So I don't think I have a pull-up or down? Is it OK for that to be the case with LPUART pins? I don't get any errors after resetting my board, if there are they are code-related.
I've set my inputs as pull-downs.
I'm quite a novice and really don't have a lot of technical know-how.
2021-09-28 7:41 AM
Example1: I have boards with a header that allows connecting an FTDI UART 3.3V cable, so the MCU needs pullup on UART_RX when cable not connected
Example2: USB VCP
Paul
Paul
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.