STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Programming secondary chip using SWD interface

HiI have a chip in main board that can be programmed using SWD interface.Can I use the SWD of the STM32F407 to program another chip (and not just for programming and debugging the STM32) ?If so - Are there any HAL functions ?Thanks

Ofer by Senior
  • 7652 Views
  • 15 replies
  • 0 kudos

core to core event interrupt

Hello,I am working on Nucleo-h745ziq board. I enable cm4 to cm7 event and cm7 to cm4 .I enable the timer in cm4 and cm7 .But the event it doenot occur in cortex m7 ,my programme is below please help me.void HAL_TIM_PeriodElapsedCallback(TIM_HandleTy...

MDeva.1 by Associate II
  • 1539 Views
  • 4 replies
  • 0 kudos

Resolved! Possible porting from MCU STM32F746ZG to MCU STM32F767ZGT6

Hi folks,,, I would like to understand how much is the effort of doing the porting from MCU STM32F746ZG  to MCU STM32F767ZGT6 ...How many changes I should made?Thanks a lot for this information but now the situation with the supply of micro as you kn...

SGasp.1 by Senior
  • 2268 Views
  • 4 replies
  • 0 kudos

Resolved! How to use a same uart for two devices

Hello every one , i'm using a STM32L100RX, i am using PC11 and PC10 ports as USART3, so far everything it's okay, but i need to use the same usart (USART3) on the PB11 and PB10 pins...i need configure these pins in runtime because i have another devi...

RComa.1 by Associate II
  • 3963 Views
  • 10 replies
  • 0 kudos

Resolved! Sync problems between H7 cores

hello!i am working with the stm32h745 dual core nucleo dev board.currently, i am trying to create a constant pulse on a GPIO output pin which belongs to the M4 core every 40 ms.when i run with the m4 alone the pulse is very accurate and looks perfect...

yuri CH by Senior
  • 1587 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.