STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Programming sequence error occur randomly on STM32H750

Hi guys,I am using the STM32H750 and try to reprogram the internal 128KB flash.Please check my code as below :During the programming i got the "PGSERR" randomly , and error code is "0x00040000 "Any comment , thanks HAL_FLASH_Unlock();  __HAL_FLASH_CL...

fema by Associate III
  • 3046 Views
  • 4 replies
  • 0 kudos

STM32H7 QUADSPI Status Polling in 444 Mode

I'm noticing some odd behaviour in the QUADSPI peripheral on the STM32H743. When I use the automatic status polling feature in quad mode it appears that the 1st query works as configured, but subsequent queries are strangely incomplete.What I mean by...

0693W000003QUQOQA4.png
MWalk.3 by Associate II
  • 1414 Views
  • 1 replies
  • 0 kudos

Resolved! Using TIM3 in STM32H753 to trigger BDMA

Hi,I'm trying to generate a serial data pattern in STM32H753 for WS2812B LED chip. I did it before with STM32F2, as the TIM, GPIO & DMA2 are within the same data bus matrix, i'm able to use TIM module events as a trigger event for DMA, and start movi...

JLee.46 by Associate II
  • 1840 Views
  • 2 replies
  • 0 kudos

STM32F4 and alternatives

Hello everyone ; Please if someone from ST could confirm : We have a shortage of stm32f429 and the given lead time is about 80 weeks ; so our production will be stopped for 1 year; to solve this we decided to revise the design of the board and cho...

Resolved! STM32L452 ADC shifted

STM32L452 ADC1 single-mode works with DMA1. ADC results are higher than the actual Voltage by around 25%. Any possible directions?

IP.2 by Associate II
  • 1506 Views
  • 2 replies
  • 0 kudos

Resolved! Is there any STM32H7 reliable emulator?

Hi everybody,I'm working on the stm32H747/757, and later will work on STM32H753.We have a test-driven development attitude and I was curious, is there any way to emulate the MCUs of H7 series?Thanks all :) 

AAvda.1 by Associate II
  • 6322 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.