STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Reference manual RM0008 for STM32F107xx outdated or wrong?

The STM32F107Vx has 2 CAN interfaces.In the TRM RM0008 Rev 21 dated February 2021 on page 115 I can only find one entry to enable the CAN clock, bit 25. What CAN clock does this bit enable? CAN1, CAN2 or both? Or does the reserved bit 26 enable CAN2 ...

fxrb by Associate II
  • 837 Views
  • 2 replies
  • 3 kudos

Resolved! STM32F407 decoupling capacitor 100nf or 10nf

The power supply scheme indicates to use 100nf for vref and vdd, but in the General PCB design guildines section (Figure 51 and 52) indicates that 10nf power decoupling capacitor should be placed. I am confused which capacitor is suggested for adc de...

DNI by Associate
  • 884 Views
  • 2 replies
  • 3 kudos

Resolved! JTAG STM32H757XIH6

should the pullups on JTAG should be given for JTAG in STM32H757XIH6, also are there any extra consideration taken care while using ARM JTAG. If pullup is not necessary, why is it so.

STM32L496 Sleep & Wakeup

Split from:https://community.st.com/t5/stm32-mcus-products/is-is-possible-to-wakeup-the-stm32l496-with-an-external/td-p/741267as this is a new question.Hello @STTwo-32 as the wake up pin associated with stm32L496 is SYSWKUP2 can i use this and on cli...

Abhiram_12_0-1744616362065.png Abhiram_12_1-1744616380305.png

STM32G030 RTC LSE clock instability

I tried to use internal RTC with LSE clocking in device which has GSM/GPRS module (GSM part decoupled from MCU part by ferrite beads in power lines and resistors in data lines). In first PCB revision (no separate ground region under crystal) I notice...

NiTr0man_0-1754295334425.png
NiTr0man by Associate III
  • 1909 Views
  • 16 replies
  • 1 kudos

Resolved! STM32N657 - eMMC issue

Hello,Our board has an STM32N657 MCU connected to an IS21S08GA eMMC.We use an 8-bit bus, and SDMMC1 is configured to run at 32 MHz.In polling mode, read/write operations work, but are very slow — it takes about 1–2 ms to read or write a single block ...

Resolved! ST-Link not properly resetting STM32

Hi,I am trying to solve a strange programming related problem I am now having after updating the reset circuit of my STM32F439-based board. Below is a comparison between my old and my new circuit:The reason I made these changes is because this is a l...

GerhardLnf_0-1754651699616.png

STM32N6 Debug Jump From FSBL to Secure Application

Currently, I have a project using a secure application for the STM32N6570-DK. I am able to run and debug the FSBL and Application with the system in Dev Boot, but have yet to be able to attach and debug when booting from the external flash (Boot1 and...

aroby95 by Associate II
  • 2598 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.