STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Problem rewriting Macronix flash

Using STM32H7B3I Discovery for program development.Using stm32h7b3i_discovery_ospi.c thus BSP_OSPI_NOR_*** functions.Which uses mx25lm51245g.c thus MX25LM51245G_*** functions.Which uses stm32h7xx_hal_ospi.c thus HAL_OSPI_*** functions.Can erase relia...

SPI Master-Slave Communication

Hello,I want to communicate with SPI between STM32F7 and Texas DSP devices. STM32F7 is the master device and Texas DSP is the slave device. I am sending data from STM32F7 master device to Texas DSP slave device. But I can not send data from slave dev...

Subtle Q on 32F4 dual DAC (32 bit data feed) mode

I am finding that with DAC1 triggered from TIM5, DAC2 can be set either for the same trigger (the doc implies that) or for no trigger ("software" trigger). Both work.I would have expected software trigger / no trigger to work on DAC2 because the 32-b...

PHolt.1 by Senior III
  • 3739 Views
  • 13 replies
  • 0 kudos

NUCLEO-H745ZI-Q doesn't runs my program

Hello,I've ordered two NUCLEO-H745ZI-Q at a same distributor, on a same time.It seems that one CPU's board is "bricked" : The software runs fine on a board. the same software literally doesn't run on the second board.The embedded debugger tells that ...

ADe C.2 by Associate
  • 1371 Views
  • 2 replies
  • 0 kudos

SPI DMA STM32H742VI with LL with Polling

Hello,I have tried to implement a simple SPI driver. Only with LL Lib. I would like to use DMA and I will do it without interrupts.So it works now. But for me it is not clear how to poll if the transfer is finish in the right way.So I use rx and tx d...

STM32H7 , Very slow processing time ?

Hello, i am using stm32h723zg nucleo board in my project. my system clock frequency 480 MHZ, that means it does an instruction for about 2,08 ns as well but the time i measure9-10 ns , That's too much.(application ; Writing adc value to another v...

0693W00000GZ1UQQA1.png 0693W00000GZ1U1QAL.png

Find out a wakeup source on STM32H7

Im trying to put STM32H743 in stop mode with wakeup from external interrupt. So far core wakes up immediately afterHAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFE);EXTI_CPUPRx registers all set to 0, so what wakes up the CPU? Is the...

Resolved! [SOLVED] NUCLEO F207ZG TIM6 timer half speed using CMSIS

Hello, I need to perform some task without using HAL libraries. I am using CMSIS. To start, I have set up a blinking led with timer. I programmed the clock as per attached picture. The source clock of TIM6 should be 60 MHz but the led behaves as it w...

ABert.5 by Associate II
  • 3194 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.