STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

defined things called "undeclared"

Hi, my processor is STM32L010C6TX. I added function to my project to use microsecond But " DWT" "CTRL" etc. It says not defined. However, they are all in the "core_cm4.h" library. This library is in Drivers-> CMSIS->Include. why doesn't it call this ...

ZKURT.1 by Senior
  • 10577 Views
  • 9 replies
  • 0 kudos

8 timers of 2 Stm32f7 Synchronization

Hello everyone,I have used 2 Stm32f7 nucleo boards to read the data of 8 incremental encoders. for this purpose, I have used timers. I can read the data of encoders correctly but there is a little bit time difference between timers. it means I need t...

Nmo.1 by Associate III
  • 2941 Views
  • 8 replies
  • 0 kudos

STM32H747I LQFP176 Package Pin-out mistake in datasheet

The LQFP176 Pin-out at Page no.76 of STM32H747I in datasheet (DS12930 Rev 1) has a mistake at pins 158 & 159.Pin 158 has been mentioned as VSS instead of PG14.Pin 159 has been mentioned as PG14 instead of VSS.But at Page no.86 these 2 pin functions a...

Resolved! The difference between VREF+ and VDDA of STM32F407

Is the following note quoted from the specification of STM32F407 applied to all the time from power-up or just during the period when the analog data is being sampled?「4. If VREF+ pin is present, it must respect the following condition: VDDA-VREF+ < ...

捷鄭.1 by Associate
  • 1730 Views
  • 2 replies
  • 1 kudos

I need to transmit two buffer trought HAL_UART_Transimit_DMA. I wrote in the code two consecutive command to do it but when I run the code, HAL_UART_Transimit_DMA do not return HAL_OK. It return HAL_OK only in debug mode stepping with F6. Why?

uint8_t slv_add[] = {0xF1, 0x0A, 0x00, 0x57, 0x53};                            if(HAL_UART_Transmit_DMA(&huart1, &slv_add, (sizeof(slv_add)/sizeof((slv_add)))) != HAL_OK)Error_Handler();uint8_t cell_sel[] = {0x91, 0x00, 0x0D, 0x06, 0xA8, 0x6E};      ...

GMart.6 by Associate II
  • 1505 Views
  • 2 replies
  • 0 kudos

Resolved! i2c to communicate two STM32F103C8T6

hello,i am trying i2c to communicate two stm32f103c8t6 . It is not working. logic analyzer output is shown in picture.what can be done for i2c to communicate two stm32f103c8t6 address 0x00

0693W00000HoeKxQAJ.png
SSaya.1 by Associate II
  • 2265 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.