2021-12-16 12:21 AM
Is the following note quoted from the specification of STM32F407 applied to all the time from power-up or just during the period when the analog data is being sampled?
「4. If VREF+ pin is present, it must respect the following condition: VDDA-VREF+ < 1.2 V. �?
Solved! Go to Solution.
2021-12-16 1:13 AM
Welcome, @�?� 鄭, to the community!
the note applies to the entire time when Vref is present and not only when analog data is sampled.
Regards
/Peter
2021-12-16 1:13 AM
Welcome, @�?� 鄭, to the community!
the note applies to the entire time when Vref is present and not only when analog data is sampled.
Regards
/Peter
2021-12-16 1:28 AM
Thanks for your prompt reply. Then I will generate Vref and VDDA from the same source.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.